Part Number: TMS320F28334 Dear Sir ,
we have old product that use the c2000 TMS20F28334ZAYA , due to component shortage can we use TMS20F28335ZAYA instead
without changing the software (it have the same pinout / functionality ) , the only difference…
Part Number: TMS320F28334 GPIO pins 84,85, 86 & 87 are connected to 3.3v through 22k pullup resistors. The system always boots properly from the emulator, but with the emulator disconnected and cycling power, sometimes it boots and sometimes not. These…
Part Number: TMS320F28334 I am using GPIO20 thru GPIO24 and GPIO50 thru GPIO58 as inputs. They are all configured as inputs,and all work properly with the exception of GPIO22 & GPIO52. Is there something different about thes two GPIUO points?
Part Number: TMS320F28334 Other Parts Discussed in Thread: C2000WARE Hello Guys,
Good day.
Our customer is using CCS v3.3 on TMS320F28334. Is there a piece of software that they can install in their panel PC that will connect permanently via USB cable…
Hi G,
Please stop asking for the F28334 kernel. I explained this to you months ago. The difference in these two part numbers does not effect the SCI flash kernel. The F28335 is the superset device and the F28335 SCI kernel is identical to the F28334…
Part Number: TMS320F28334 Dear team,
we would need your help to look into the following case where
The problem description is the following; signal XCLKOUT is missing at any time and they believe that uC has no clock.
They do not have idea what…
Part Number: TMS320F28334 Other Parts Discussed in Thread: C2000WARE Hi Guys, man I have not been here in a while.
Anyway, I'm starting a new project using the TMS320F28334 which I will be receiving a few chips in a few days, so I thought I'd get CCS…
Rajkumar / Jyoti,
Problem resolution: Application that was getting programmed in flash was using Sector H / G. But, serial flash programmer software wasn't erasing Sector E / F / G / H before trying to program the new application code that is the reason…
Part Number: TMS320F28334 Other Parts Discussed in Thread: TMS320F28379D , TMS320F28388D
Number: CS0308807: Advice about DSP selection
I need to select a DSP for our future magnetic bearing controllers of our own manufacture and design and programming…
The CCS project migration feature does not guarantee the resulting build matches the previous build. While we are not specifically aware of issues with regard to the --opt_for_speed option, it is not surprising that minor differences occurred. The only…