Part Number: TMS320F28335 Hello,
The TMS320F28335 chip solder ball has the following issues, resulting in virtual soldering during soldering. Please help to check if there are any changes to the welding process and conditions. It can avoid the problem…
Part Number: TMS320F28335 Other Parts Discussed in Thread: TMS320F2812 Hello, Im Brendan.
I'm currently attempting to perform standalone firmware downloads for mass production of the TMS320F2812 and TMS320F28335 using the S-GANG programmer.
Since…
Part Number: TMS320F28335 Hello TI C2000 experts,
I am debugging an issue on a TMS320F28335 where the DSP occasionally hangs during an XINTF read access to external RAM .
System description
MCU: TMS320F28335
External memory: RAM connected through…
Part Number: TMS320F28335 I’m troubleshooting an intermittent, self-recovering CAN communication dropout on a field-deployed system with TMS320F28335 DSP (Rev 0/A) and two Xilinx Spartan 6 FPGAs. The failure points strongly to a known TI eCAN silicon…
Part Number: TMS320F28335 Hello,
I am currently working on migrating my development environment from CCS to Antigravity (VS Code-based IDE) for a project using the TMS320F28335.
So far, I have successfully configured the build system using CMake and…
Part Number: TMS320F28335 Hi TI,
I am working with the TMS320F28335 MCU and I am facing an issue where the internal watchdog is continuously triggering, which is preventing me from connecting via JTAG. I had previously flashed some code to the Flash…
Part Number: TMS320F28335 Hi, All,
I'm encountering a problem with the TMS320F28335. This product entered mass production in 2021 and has been working smoothly until recently, when some customers returned units for repair.
The reason is that the TMS320F28335…
Part Number: TMS320F28335 Hi Team,
1. Poor production testing, approximately 6% defective 2. As shown in the figure below, confirm that pins 100 to 89 are faulty (no defects were found in other pins). These pins are all used as input I/O. Voltage changes…
Part Number: TMS320F28335 I am recieving a float number from CAN bus, but the nubmer is smaller than F_MIN, about 1e-42, but as soon as I assign it to a long double or a float, it becomes 0. So I tried to use the following function to convert, but still…
Part Number: TMS320F28335 Other Parts Discussed in Thread: CONTROLSUITE Hello, My name is Kwangsu Kim, and I am a senior researcher currently developing with the TMS320F28335.
I am reaching out regarding an issue related to the CAN communication functionality…