Part Number: TMS320F28374S Hello, all.
since MCUs DCSM mosule dosen't have JTAG lock implemented(according to manual) the best alternative we found is locking everything in same DCSM zone. The problem we encountered is that this way does not support locking…
Part Number: TMS320F28374S Hello,
According to https://software-dl.ti.com/C2000/docs/c28x_interrupt_nesting/html/index.html the structure of a nested interrupts is as following:
void EPWM1_TZINT_ISR ( void )
{
uint16_t TempPIEIER ;
TempPIEI…
Part Number: TMS320F28374S Other Parts Discussed in Thread: C2000WARE Hi Team,
There's an issue from the customer need your help:
I created a project on CCS and used it on the TMS320F28374s chip, but a structure variable in the project has not been…
Part Number: TMS320F28374S Hello,
Is it allowed to use interrupt vectors which are descriped as "reserved" in the correspointing PIE Interrupt Vector table?
For example to use interrupt vector INT12.4 (Group 12 channel 4)?
I want to trigger…
Part Number: TMS320F28374S Other Parts Discussed in Thread: C2000WARE When F28374S is upgraded online, the upgrade will fail. The specific process is as follows:
F28374S BOOT program description:
1) F021_API_F2837xS_FPU32.lib is allocated to the BOOT RAM…
Hi Ken, thanks for your patience while I was out of the office.
Ken Lai said: 1. Is STA_RAM_LOGIC_TEST and STA_RAM_DETECT can work on RAM_M1 which be allocated to .stack in memory map?
There are complications with using the RAM test mode on the memory region…
Hi Ben,
Yes if TBPHS is set to a value greater than TBPRD the TBCTR will never reach TBPRD. The sync event will cause the TBCTR to set to whatever value you chose. Then the TBCTR will start incrementing.
Ben Qin said: In addition, in the up-down counting…
Part Number: TMS320F28374S Hi team,
Use SCIB for 485 half-duplex transmission, SCIB does not use interrupts, the main flow always queries, and the baud rate is 115200. The upper computer (PCs) periodically sends one byte of data to the TMS320F28374S,…