Part Number: TMS320F28375D Other Parts Discussed in Thread: C2000WARE Hi
May I have question about F28375D CPU Timer?
My customer set as this:
CPU Timer 0
・interrupt every 100 ns
・not set prescaler
・In interrupt function, GPIO is high (for debug)
CPU Timer…
Part Number: TMS320F28375D
Hi
May I have question about F28375D Vdd maximum current?
I think Vdd (1.2V) is DSP core voltage.
Is this current (Idd) incread by only CPU operations? e.g. CPU frequency, crystal circle, PLL config.
And is the peripheral operation…
Part Number: TMS320F28375D
Hi,
I have a C code written for the CLA task. And I wish to write asm instructions as well.
I want to toggle GPIOs which are gate signals to a power converter. In order to implement delay I want to include the asm("MNOP") instruction…
Part Number: TMS320F28375D Hi experts,
Is it possible for you to tell me the detailed conditions under which the return value is 1 after executing SFO() on C2000?
I understand from TRM[15.14.2 SFO Library Software] that 1 is returned if "MEP_ScaleFactor…
Part Number: TMS320F28375D Hi
May I have question about F28375D pin connection.
My customer is using F28375D PTP 176-pin package.
-----about Flash test pin-----
Q1 :
I think FLT1(73-pin) must be unconnected.
But, If connected to 3.3V Before POR, Device…
Part Number: TMS320F28375D Hi experts,
I have a question about TBPRDLINK in the EPWMXLINK register. My customer when initializing PWM, PWM8's TBPRDLINK is set to the register values stored in PWM7's TBPRD and TBPRDHR.
Q1:How long does it take to…
Part Number: TMS320F28375D Hi
May I have a question about F2837xD datasheet?
In 8.10.1.2.4 ADC Characteristics,
https://www.ti.com/lit/ds/symlink/tms320f28375d.pdf
How was the test temprature?
And the max value of errors (e.g. gain error, offset error…
Part Number: TMS320F28375D Team,
Customer got 5u samples from TI.COM store but the IC marking is not what we document in the marking nomenclature from the datasheet. Can you please confirm that those IC are really TMS320F28375DPTPT? (I guess there were…
Part Number: TMS320F28375D Hi All,
We used TMS320F28375D as our microcontroller. We also used HIL for test and debug. We used a btd file to run microcontroller on our circuit board. Now we used TI XDS110 debug probe to collect more intermediate variables…