Part Number: TMS320F28375D
Team, I have attached a sim file. Is it possible to directly interface the output of isolator to the controller ADC in differential mode.
FYI, +1.5V available in my board
ADC VREFHI: 3V
ADC VREFlow: 0V
Discussion.TSC
Part Number: TMS320F28375D Hi All,
We used TMS320F28375D as our microcontroller. We also used HIL for test and debug. We used a btd file to run microcontroller on our circuit board. Now we used TI XDS110 debug probe to collect more intermediate variables…
Part Number: TMS320F28375D Customer asking about HWBIST procedures executed in boot ROM.
After CPU reset from CCS debugger, or power cycle on/off the CPU2 doesn’t boot correctly – here are recent observation (screenshots are form spruhm8i – 2837XD TRM…
Part Number: TMS320F28375D Other Parts Discussed in Thread: SYSCONFIG , C2000WARE
Hi,
We are considering developing a new product using the F28375D software. Due to board area limitations, we are considering replacing with small pin package piccolo series…
Part Number: TMS320F28375D Customer set cpu2 to go to main after reset but it doesn’t work (for cpu1 it works)
When they set script: Scripts->EMU Boot mode select->EMU_BOOT_FLASH then it works for cpu2 too but after re-loading program to cpu again…
Part Number: TMS320F28375D Hi. I am working with tms28375d microcontroller. I am trying to use 200MHz system clocking, however i am running into problem when i am trying to run the code on CPU. I am getting the following error if i try to set exactly 200MHz…
Part Number: TMS320F28375D
We have question about INT16/INT32 multiplication by “-1” but given by minimum negative number:
Is this CPU limitation or compiler error that result value is not changed ?
PS.
In limits.h we have minimum values…
Hi Mayur,
We are closing this post since we did not hear back from you.
If you have further questions, please open a new post.
Thanks and regards, Vamsi
Part Number: TMS320F28375D Other Parts Discussed in Thread: C2000WARE Hi,
I am trying to run flash example from C2000Ware 3.03 (device_support\f2837xd\examples\cpu1\flash_programming_dcsm\cpu01).
But after going to the example function Example_CallFlas…
Hello Vamsi
My name is Trung Dao.
I wrote boot code to program OTP this device.
The other location in OTP work fine. However we have issue to program 0x7801E(1-BOOTCTRL). After programmed still have 0xFF.
The function for program :oReturnCheck = Fapi_issueProgrammingCommand…