Part Number: TMS320F28376S Other Parts Discussed in Thread: C2000WARE
Hello everybody, I have a problem, with sending the firmware with SCI using the example version called (F2837xS_sci_flash_kernel),
I put the recommendations seen in other posts here…
Part Number: TMS320F28374S Other Parts Discussed in Thread: C2000WARE
Hello!
Need help to create bootloader for TMS320F28374S through SCI connected through RS-485 (sn65hvd1781aqdrq1)
What software I can use for that?
What hardware to use to connect to…
Part Number: TMS320F28376S Other Parts Discussed in Thread: UNIFLASH Dear sir ,
We have controller that is based on 28376SZWT , due to component shortage we are considering to assemble 28377SZWT (which we able to buy).
I have looked at the datasheet ,…
Part Number: TMS320F28376S Dear sir ,
we are devloping Motor controller using C2000 28376S , and we want to make use of the tripzone (for short circuit) in such way
it will disable specifc PWM channels , example
TZ1 will disable PWM1.CHA PWM1.CHB PWM2…
Part Number: TMS320F28376S Dear Sir ,
We are developing Conntroler based on TMS320F28376S , and need some clarifiction regrding Singlas coming into the Chip before device gets VDD ( e.g during power UP)
the signals are up to 3.3V , but they exisit before…
Part Number: TMS320F28376S Other Parts Discussed in Thread: C2000WARE Dear sir ,
1.We are developing Motor Controler based on C2000 28376S , we need to create Complementary PWMs singlas Per Phase (total of 3 phases)
2. each Phase will connect to PWM module…
Part Number: TMS320F28376S Dear Sir ,
we are developing controller base on 28376S Chip , and using SPI communication + RS422 trancivers to communicate with extreanl end equipment
1. we recentaly came acrros endequipment that requires from us to work…
Part Number: TMS320F28376S The use of the internal 1.2V is not supportet for delfino. Regardless this requirement we misconfigured the delfino TMS320F28376S by connecting the Vregenz to VSS (board ground). We have never seen any functional problems but we…
Part Number: TMS320F28376S Other Parts Discussed in Thread: C2000WARE Dear sir ,
we are developiong motion controller based on 28376S , and using the CLA for current loop implementation , we have some calculation that need to be done in the CLA such as…
Part Number: TMS320F28376S Dear Sir,
we are devloping Controller based on 28376S Chip , and want to make use of the eQEP for supporting incremental quadrature encoder .
i have reveiew the related example for better understand , but have some question…