Part Number: TMS320F28377D Other Parts Discussed in Thread: C2000WARE , SYSCONFIG Hello Experts ,
I have a implemented independant modulation on epwm8 (EPWM8A & EPWMB).
I have some confusion on the action qualifier settings and interrupt settings.
…
Part Number: TMS320F28377D Dear expert,
Why it will not always match the actual addressing?
Is there any way to monitor the address/data for CAN on C2000?
Part Number: TMS320F28377D Hello. I had the same problem when I was working on a project. I use CCS for debugging. I stop feeding dog in CPU2, the process will stop automatically. After using the "CPU Reset" and "Restart" buttons on CCS to reload the program…
Hi all,
I could not find source code of CPU1BROM_calculateCMAC(...).
But I managed to calculate CMAC.
There is a library at the " C2000Ware/libraries/security/crypto/c28/aes" folder.
"AES_performCMAC()" function calculate CMAC successfully.…
Part Number: TMS320F28377D Hello:
Regarding the customer's power filter project, if there are any issues, please help to take a look; Thank you!
The client has been using version 6.1.0 of the compiler, but now they need to use 28377 with CLA suffix…
Part Number: TMS320F28377D I am currently developing a project using the 28377D MCU.
However, I am encountering challenges in utilizing the 16-bit ADC,
particularly when dealing with single-ended analog input signals.
My hardware's analog inputs are…
Hello Zane,
As you have already emailed the schematic review mailing list, let me know if they respond with an answer. The files you attached are not ones I can open, I was more asking for an actual image that laid out the circuit diagram connections…
Part Number: TMS320F28377D Hi Team,
Our customer want to use USB DMA to transfer data, but in TRM:
Can you provide a demo which use USB DMA to transfer data?
Best Regards,
Zane
Part Number: TMS320F28377D Other Parts Discussed in Thread: C2000WARE Dear Forum,
I asked the same question some months ago - now i have finally found the cause.
This include chain overwrites --diag_error=70 in the makefile:
#include "F28x_Project.h" …