Part Number: TMS320F28377D Hello,
I am using the TI-TMS320F28377D for a motor drive application, on core 1 I have a standard CAN-Stack and on core 2 I have the motor drive specific software, the two cores exchange information over the IPC.
Everything…
Part Number: TMS320F28377D Hi Expert,
I have some cunfsion on the adc ex6 soc continuous dma example.
First is about triggering for ADCA.
Seems that the SCO0 is triggered by PWM, and the rest of the SOC are triggered by software.
//
// Configure…
Part Number: TMS320F28377D Tool/software: Dear TI Support Team,
I am currently developing on the TMS320F28377D device and using the Flash API function: oReturnCheck = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, (uint32 *)Bzero_SectorN_start…
Part Number: TMS320F28377D Tool/software: oReturnCheck = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, (uint32 *)Bzero_SectorN_start);
Before and after the code was executed, the oscilloscope was measured using the GPIO function. The total run…
Part Number: TMS320F28377D Tool/software: Hi,
The TMS320F28377DPTPT received by the customer has a small dot in the middle of its appearance. Could you please help confirm the cause?
Thank you~
Part Number: TMS320F28377D Tool/software:
where i can config the build-configurations like old version CCS?
In ccs20.2 I only can only find to create new build-configuration based on CPU1_FLASH and CPU1_RAM. but I can't see the specific configyrations…
Part Number: TMS320F28377D Hello,
I am using the TMS320F28377D for EtherCAT on my device and I am having an error when I try to add a new object to my object dictionary.
I have already almost 50 objects added, but these last few objects are giving…
Part Number: TMS320F28377D Tool/software: Dear, experts
Since I can't use SCI Bootloader using SCI0-Boot(GPIO84, GPIO85),
I'm trying to use SCI1-Boot(GPIO28, GPIO29) to run SCI Bootloader.
I set it to operate as SCI1-Boot by setting 0x0000815A or…
Part Number: TMS320F28377D
Tool/software:
Hi Expert
Customer organizes the dual core project in order below:
CPU1: Customer_boot_1+APP_1
CPU2: Customer_boot_2+APP_2
The program can free run without emulator, but once connect the XDS100V3 to…
Part Number: TMS320F28377D-Q1 Tool/software: Hi,
Our customer is using 12 Bit single ended measurement.
Over all got an error of 12 LSBs (Gain error 5 + Offset error 4 + DNL 1 and INL 2). Is this error over whole temperature range and lifetime?…