Part Number: TMS320F28377D-EP Other Parts Discussed in Thread: TMS570LC4357-SEP , , HALCOGEN , C2000WARE , TMS320F28377D , SYSCONFIG Tool/software: Hello Team,
We are exploring the above mentioned microcontrollers ( TMS320F28377D-EP and TMS570LC4357…
Part Number: TMS320F28377D-EP Tool/software: I would like to konow bellows.
Please inform me.
1. Supply ramp rate
About: supply ramp rate requirement in Datasheet 4.7.1 table 4-3
Question: Is the requirement applied to only power-on state or power…
Part Number: TMS320F28377D-EP Hello,
Our customer has the inquiries below. Would you help address them?
I am working on a sin/cos encoder interface. Using a launchXL dev board we were able to get the interface working. The question is:
We had…
Part Number: TMS320F28377D-EP The datasheet has the table below, but when considering a two-resistor model, which thermal resistance should be applied?
RJC and RJB ?
PsiJT and PsiJB
Part Number: TMS320F28377D-EP Tool/software: Hi,
We would like to use the CPUs as follows:
CPU1: FLASH Boot, CPU2: Not Used There is no image in CPU2's flash, and we only want to boot from CPU1's flash.
1. If we don't execute the "IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH…
Part Number: TMS320F28377D-EP Tool/software: Hello,
I am using TMS320F28377D-EP in my product. In my Firmware, the ADC gets SOC from 2 sources: one is via EPWM module (PWM-synced Interrupts) and another is SW-triggered SOC (Force SOC operation). These…
Part Number: TMS320F28377D-EP Other Parts Discussed in Thread: SEGGER Tool/software: Hello,
Does Segger J-Link Pro supports TMS320F28379D-EP Microcontroller?
Nilesh Karale
Part Number: TMS320F28377D-EP Tool/software: We are using TMS320F28377D-EP processor for communicating with ARINC chip through SPI. The Chip is connected to SPIB with 4 wire and SPI is configured for 8bits.
We are able to establish the communication…
Part Number: TMS320F28377D-EP Tool/software: Can I assign SOC0 to multiple ADC channels from different ADCs?
For example Ax Bx Cx and Dx can they all be assigned to SOC0
Part Number: TMS320F28377D-EP Tool/software: Could you please infrom me the 1st resonace frequency of bellow Power supply line at your PKG.
( If you have.)
/ 1st resonace frequency of Vdd to Vss
/ 1st resonace frequency of Vddio to Vss
/PKG: QFP…