Part Number: TMS320F28377S
Hello,
In the electrical characteristics, the pin leakage for DACOUTx is specified as 66uA.
Since these are shared pins, does this leakage current apply to these pins only when they are being used in DAC Output mode OR when…
Other Parts Discussed in Thread: TMS320F28377S , ADS8586S We have project where we intend to use the ADS8586S with the TMS320f28377S via the uPP module.
Is this even possible?
Please help.
Part Number: TMS320F28377S Hello TI,
My team is planning on creating a flash driver in our application to program and erase flash. Our application code will need to be certified and so the flash API library cannot be used; source code files are needed…
Hareesh Janakiraman said: If this happens, the WD would reset the device and the PLL locking process will begin again.
I downloaded the version 5 and did not see the Watchdog is enable before entering the LOOP (it is the same with version 4.01), so to…
Part Number: TMS320F28377S Other Parts Discussed in Thread: UCC2895
I wanted to realize Cycle by cycle trip using CMPSS and epwm module. where the CMPIN1P is fed externally and compared with a DAC value to generate the trip signal. I referred the example…
Part Number: TMS320F28377S Hi,
Some doubts about GPIO input qualification,
1) In the picture below, what's the sample point? If the GPIO signal's frequency is higher than sample window, what happens?
2) The sampling window is 6 samples, but actually…
Part Number: TMS320F28377S Other Parts Discussed in Thread: C2000WARE Dear Sir/Madam
On a separated thread about the PLL not locking properly we have been provided with the following screeshot as the workaround applied to the C2000Ware lib
( https://e2e…
Part Number: TMS320F28377S Dear Sir ,
We are using TMS320F28377S in our application .
JTAG SIMLUATOR XDS100. or XDS200. for TMS320F28377S ? which one is better and why