Part Number: TMS320F28378D Hi, I'd like to know the response time of the TZ function.
According to the TRM(TMS320F2837xD, p1913),
"When a cycle-by-cycle trip event occurs, the action specified in the TZCTL[TZA] and TZCTL[TZB] bits is carried out…
Part Number: TMS320F28378D Other Parts Discussed in Thread: UNIFLASH Hi,
What's Window's system level requirement for F2837xD Uniflash programming?
On Win7 (32bit and 64bit) systems, the latest Uniflash can be used to program F2837xS successfully…
Part Number: TMS320F28378D Hello,
We plan on using the TMS320F28378D, do you have data on the junction-to-case top thermal resistance available?
This would be important for us to pick the right thermal pad on top.
Thank you and best regards,
Ambroise
We will have many DSP, possibly up to 15, all connected together using the McBSP in TDM mode. Since the environment is little noisy we intend to use M-LVDS. So each DSP has to activate his external M-LVDS data buffer during their respective time slot…
Part Number: TMS320F28378D Hi,
I have noticed that on the same bridge, CPU1 and CPU2 are connected. In the case of CAN CPU1/CPU2 selection is done with CPUSEL8.
If the 2 CPUs access 2 different CAN at the same time, Is there a time arbitration?
Best …
Part Number: TMS320F28378D Hello Everyone,
Good day!
Currently running the dual_axis_servo_drive_fcl_qep_f2837x project and I am in build level 4.
During the calibration process the motor turn at least 90 to 120 degrees. But after the calibration
the…
Part Number: TMS320F28378D I've flashed both CPUs on the microcontroller to boot in standalone operation. When power is cycled to the microcontroller, the desired results is to have both CPUs start up and begin running. Sometimes after a power cycle…
Part Number: TMS320F28378D Hello guys,
What is the main difference between F28378 and F28379? When I use TI website to compare, I see that they are more or less the same except ADC (see below). F28378 suppports only 12 bit adc while F28379 supports 12…
Part Number: TMS320F28378D Hi Guys, on the IT website it says that the new TMS320F28378D can run at 800MIPS, does that mean that the I/O PORTS run faster too?
The 8387D datasheet says that the I/O ports run at a top speed of 25Mhz and I'm wondering about…
Part Number: TMS320F28377D Other Parts Discussed in Thread: TMS320F28379D , TMS320F28378D , , TMS320F28375D , TMS320F28374D
Hi all,
in device documentation there is a chapter "Identification" which contains following table:
NAME
ADDRESS
SIZE…