Hi Rajamurugan,
1. You can consult the DCSM section in the SysCtrl chapter of the TRM and look up other posts on E2E to check if you're seeing a similar issue.
2. You can unlock the DCSM and look at the OTP locations (0x78000 to 0x783FF) to check…
Part Number: TMS320F28379S
Tool/software:
Please see attached CCS project (testDSSWS.zip) and DSS script (read_symbol_values.txt..you will need to change the extension to .js).
The output of the script is shown below.
>C:\ti\ccs1210\ccs\ccs_base\scripting…
Rajamurugan,
Rajamurugan Kaleeswaran said: However, when I try to upload both the kernel file and the application code through SCI mode, it doesn't branch to the application code from the kernel.
Why do you think it isn't branching to the application…
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE Tool/software: Hi,
I was told (see here: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1437388/tms320f28379s-jtaglock…
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE Tool/software: Hi TI team,
I'm using the TMS320F28379S on a custom PCB and have configured the device to boot via SCI boot mode using boot select pins . While the bootloader does…
Hi Alex,
Sure! will open a new thread regarding this issue.
link - https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1498424/tms320f28379s-controller-not-branching-to-application-after-sci-bootloader…
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE ,
Tool/software:
Major concern :- 1. Detailed steps to change BMSP0 to GPIO73 in Z1_BOOTCTRL and leave others to default ?
2.To test this I need to try EMU boot mode what…
It is working now. I needed to write to the flash twice. I took the DCSM files (asm and cmd) files sysconfig generated and removed the zone configuration section as shown below. I also removed the DCSM configuration from sysconfig.
;------------------…
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE Tool/software: C2000Ware_5_04_00_00 does not have an example using the F28379S CAN with message objects configured as a receive FIFO.
Please provide example code of configuring 5 message…