Part Number: TMS320F28379S
Hi all,
I'm using the controller TMS320F28379S for my application I'm using all the 20 Analog inputs, I need to know, how much does the ADC required to given me the result (ADC Conversion time) ?
ADC is triggered using…
Hey Jeremy,
Adding a .syscfg file to a bitfield example such as blinky_with_DCSM won't work, since SysConfig is built on top of driverlib. Could you try the following steps instead?
import the emtpy_bitfield_driverlib_project from the device_support…
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE Hi All,
I want to use GPIO_SetupPinMux & GPIO_SetupPinOptions and I need to know more about how to use it.
Example : GPIO_SetupPinMux(70, GPIO_MUX_CPU1, 0);// Pin mux option GPIO_SetupPinOptions…
Part Number: TMS320F28379S What is the lead-time and Life-Cycle of TMS320F28379SPTPS ? Also regarding the technical support.
Is it recommended for a new design?
I don't see Inventory in Suppliers' website.
Regards,
Shai
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE Hello,
In PMSM FOC control application I would like to use overmodulation.
Because of that there will be period when Low-Side Mosfet is not switching (High-Side Mosfet Turned on for…
Part Number: TMS320F28379D Other Parts Discussed in Thread: SYSCONFIG
Does TI have a text file or database that describes all the TMS320F28379's pins (pin number, functions and etc)?
I already understand the datasheet has all the pin configuration…
Part Number: TMS320F28379S Hi,
While checking the data inside the chip through real-time debugging (JTAG) , I found that there was some error (not exactly matched) between the data displayed in Expressions and Graph view and the actual data stored inside…
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE
We designed a custom motor driver board based on the TMS320F2879D. During our last production cycle there was a parts shortage and needed to substitute the TMS320F2879S processor instead…
Part Number: TMS320F28379S Other Parts Discussed in Thread: TIDA-01606 , C2000WARE I am working on custom inverter hardware trying to run the closed-loop current test with a load of 10 ohms per phase connected in a wye formation at the output.
For testing…
Part Number: TMS320F28379S System details :
I am using TMS320F28379s C2000 series micro controller and I’m trying to sync the PWM pulse between the two micro controllers considering one as a master (which sends the PWM_SYNC_OUT pulse) and another as…