Part Number: TMS320F28384D Other Parts Discussed in Thread: SEGGER Tool/software: Would TI consider working with Segger to add Jlink debug probe support for the C2000 series microcontrollers?
I found an interesting thread on Segger's forums saying they…
Part Number: TMS320F28384D Tool/software: Hello,
We are planning to use DSS for testing software requirements. This requires setting a breakpoint, update input variable, running the software to the next breakpoint, and reading the output variable. The…
Part Number: TMS320F28384D Tool/software: Does the NMI in TMS320F28384D reset the CPU or simply drive the ERRORSTS Pin low? If the CPU is not reset by the NMI, then it would be advisable to utilize the ERRORSTS Pin for resetting the CPU.
Part Number: TMS320F28384D Tool/software: Hello, I am currently using the above DSP to control a half bridge board. My problem is that I have found that both mosfet gates of my half bridge are driven at the same time during power up of my DSP board and…
Part Number: TMS320F28384D Tool/software: Hi champs,
In TRM section 37.3.8.1, the example of Transmitting Data Using SPI with DMA, to transfer 128 words to SPI using the DMA as below,
NUM_WORDS: 128
TXFFIL: 8
DMA_TRANSFER_SIZE: (NUM_WORDS /TXFFIL) …
Hi Jordan,
We usually recommend setting VCO a little higher, which in this case would be 480MHz (and then divide down by 4 to get to your CMCLK), but this is not mandatory. You are within spec either way, and your solution should be good to go.
It is…
Hello Jon,
Apologies for the delayed response; I was out of office last week. If I have understood the schematic correctly, you have a total of 6.58uF of capacitance on VDD12. This is quite a bit lower than the minimum spec of 20uF. Ideally, here you…
Part Number: TMS320F28384D Tool/software: Hi,
I believe spruii0f is the latest tech ref manual for the 2838x family. In Table 28-5, there are no options to use the SOCB of any ePWM. Instead, according to the table there are two options for each EPWM…