Part Number: TMS320F28384D Dear Sir ,
1. We are developing a controller based on TMS320F28384D , and would like to interface to FPGA using the EMIF that is configured as asynchronous 32-bit Data / 12-bit Address
2. on a previous designs we had similar…
Hi,
Could you try forcing TRSTn high with a pullup resistor? I would be curious if that changes the behavior at all. Otherwise I think the next step would be to try swapping out the C2000 device.
Best Regards,
Ben Collier
ChungWen,
If the things you specified when initially applying the QKIT change then you must re-apply the QKIT. For example, any of below would require applying the QKIT again: changing compiler options that impact code generation (ie opt_level, changing…
Part Number: TMS320F28384D In the TRM : TMS320F2838x Real-Time Microcontrollers With Connectivity Manager TRM (Rev. D) p age number 2832, there is a OR gate with entry HRFRC[CALIBDONE] which feeds the set of LATCH, and HRFRC[CALIBDONE] also feeds the clear…
Part Number: TMS320F28384D Other Parts Discussed in Thread: SYSCONFIG Hi champs,
Can MPU be used to protect the memory(flash/RAM) of CPU1 and CPU2 please?
Regards,
Luke
Part Number: TMS320F28384D Other Parts Discussed in Thread: C2000WARE , SYSCONFIG
Hello,
we are using an F28384D cpu on a signal processing board.
We have several installed CCS12.4.0 IDE in Win7 custom directories, one on a lab PC for debug,... and the others…
Hi Hareesh,
Thanks for the link, was not aware they were the same physical register, this helps explain a previous issue we observed in more depth.
Best Regards,
Scott.
Part Number: TMS320F28384D I understand that TMS320F28384D does not support gigabit ethernet. Would you please suggest a closest TI part that supports gigabit ethernet?
Thanks
Part Number: TMS320F28384D Hi champs,
When we use archiver to generate the library of object files, this .a file will contain some information, for example build time, directories... and so on.
Is it possible to configure compiler settings and let this…
Part Number: TMS320F28384D Hi,
I am developing software using F28384D.
In order to increase the speed of the program, it is expanded to RAM and processed, and by using USB, the capacity of RAM is tight. So I'm considering using external memory. I think…