Part Number: TMS320F28384D Other Parts Discussed in Thread: SYSBIOS Tool/software: I am currently using TIRTOS. I have several HWIs in the system and am considering adding a zero-latency ISR. I am using Hwi_Params with maskSetting = Hwi_MaskingOption_BITMASK…
Part Number: TMS320F28384D Tool/software: On the TMS320F28384D DSP processor, what is the short-circuit load current of the three DAC outputs, and are they protected from damage under short-circuit loading?
Part Number: TMS320F28384D While testing the watchdog on programming - (customer use FlashAPI) the customboard was blocked.
I added the logs below:
Additional error messages:
Error connecting to the target:
(Error -1015 @ 0x0)
Device is…
Part Number: TMS320F28384D Other Parts Discussed in Thread: C2000WARE Tool/software: Hello,
I am using the example "memcfg_ex1_ram_management_cpu1,"
but I cannot find the relevant file for the IPCBootCPU2 function in the following location:
ti\c2000…
Part Number: TMS320F28384D Tool/software:
Hello, how is it possible to load all three projects for all CPUs of the F28384D (i.e., for CPU1, CPU2, and Cortex M4) simultaneously with a single click on the debug button?
Part Number: TMS320F28384D Hello TI experts! I am using TMS320F28384D.
I conducted a simple test to use CPU 1 and 2 and each CLA at the same time. The results are as follows:
Single core time=74ms Single core res =1967.704102
multi core time=18ms…
Part Number: TMS320F28384D Other Parts Discussed in Thread: SYSCONFIG , C2000WARE Tool/software: When using dual data rate transmission, it has been mentioned in the 2828x TRM that within FSI TX, the data is split into even and odd-numbered bits and sent…
Part Number: TMS320F28384D Other Parts Discussed in Thread: C2000WARE Tool/software: Hey C2000 SW Team,
I have a customer evaluating the TMS320F28384D for a new project and we are hoping you can help to provide guidance on implementing BSD-style sockets…
Part Number: TMS320F28384D Tool/software: Hi champs,
My customer has below questions about compiler CQKIT coverage test,
Is the purpose of coverage test to check whether the user code contains the compiler bug?
Should customer run user code then…
Part Number: TMS320F28384D Tool/software: Hi,
I believe spruii0f is the latest tech ref manual for the 2838x family. In Table 28-5, there are no options to use the SOCB of any ePWM. Instead, according to the table there are two options for each EPWM…