Part Number: TMS320F28384S Tool/software: Hi,
I am getting above error if i try to flash Firmware, i tried resetting the board
can you please guide on this
Thanks,
Vinay Kumar
Part Number: TMS320F28384S Tool/software: Hi,
I want to know how to do debug with both CPU 1 and Community Manager.
I have two separate files to flash in CPU1 and CM.
Thanks
Part Number: TMS320F28384S Tool/software:
Below are the first six lines of the hex file.
The image is a memory browser in CCS.
Do the hex file and memory match?
I'm developing a bootloader. I wrote the hex file through the bootloader, and I'm…
Part Number: TMS320F28384S Tool/software: Hi
I have a strange behaviour with SCIA in polling mode, the problem is present only starting the app from bootloader nor debugging it. The bootloader program SCIA for character i/o then it transfer the app…
Part Number: TMS320F28384S Other Parts Discussed in Thread: C2000WARE Tool/software: Hi
I want to create and array of uint16 from a simple CM application, then I want to copy data from CPU1 to CPU1TOCM ram and boot CM. Which are best settings to create…
Part Number: TMS320F28384S Tool/software: Hi
Is it possible to step into driverlib function? I have seen that the step line position is not correct and is not possible to understand wich is the executing line, sometimes it seems to step trought source…
Part Number: TMS320F28384S Tool/software:
Hello,
I'm working with the TMS320F2838x DK board and testing the watchdog reset functionality. The watchdog is configured in RESET mode , and when I intentionally stop servicing it, the device resets as expected…
Hi Joseph,
Joseph Dunbar said: I'm working on a custom board with custom software. I am trying to boot the MCU from flash.
To simplify the issue, can you please try flashing an example from the C2000Ware SDK? I would like to check if you experience…
Part Number: TMS320F28384S Other Parts Discussed in Thread: C2000WARE Tool/software: Hi
I'm testing a new board based on the 28384S, and I have a problem in starting two ADC module:
Hi use PWM1 to generate SOCA & SOCB (may be only one can be used…
Part Number: TMS320F28384S Other Parts Discussed in Thread: C2000WARE Tool/software: Hi
I have two osclillator one 14.7456Mhz that drives the SYSPLL to obtain 199.065.600Hz for the C28. The other is 50MHz and is connected to GPIO133, I would like use…