Part Number: TMS320F28386D Hi
We are preparing to enable the JTAG LOCK and secure boot function in F28386D chip. The configured OTP data of DCSM zone1 will be added into the .out or .hex of our bootloader, then these function can be enabled after the…
Part Number: TMS320F28386D Registers a function to be called when an interrupt occurs
Interrupt_register(INT_NMI, &nmiISR);
Question: Does map file clearly show the relationship between this INT_NMI with its handler?
Due to in the project some where…
Part Number: TMS320F28386D Hello,
I am currently designing a control system based on the TMS320F28386D microcontroller. In this system, the EMIF1 interface is mainly use for reading data from a 16-bits ADC.
The process of reading continuously the ADC is…
Part Number: TMS320F28386D Other Parts Discussed in Thread: C2000WARE
Hello,
I have imported the example project from C2000ware V 5.01.00.
I'm not able to compile the following example: enet_lwip.
The problems are the following:
I'm using this configuration…
Yale,
After discussing with our team here, two additional suggestions:
Consider moving the overvoltage protection diodes (D1107) to the op amp noninverting input, so that any noise from that network gets filtered.
Given that a shunt voltage reference…
Part Number: TMS320F28386D Hello,
I'm unable to successfully import the Xpedition symbol for the F28386DPTPQ DSC I plan on using in a design.
I need a pin table in excel form to import into my tool so I don't have to put this information in manually…
Part Number: TMS320F28386D As introduced that CLA core can run at 200MHZ, but when connect with debuger, I want to know where I can check that to confrom that the CLA core is really running at 200MHZ.
Is there the register that show this information? …
Part Number: TMS320F28386D We did the code refactoring, realize the three levels of software with some cla files instead of one CLA file with no level.
But this make the CLA task executing time increase from 3us to about 9us.
I want the timing performace…