Part Number: TMS320F28388D Hello,
A few questions on the TMS320F28388D processor reset behaviour:
In the datasheet, section 7.10.2.1 describes device subsystem behaviour during reset. It is mentioned that the IOs are high impedance. Does this include…
Part Number: TMS320F28388D Hello,
On the TMS320F28388D we plan to split SDFM1 and SDFM2 between CPU1 and CPU2 (CPUSEL4), one instance per CPU. Each CPU would also need to read one channel that is filtered on the other CPU's SDFM instance.
For the…
Part Number: TMS320F28388D Other Parts Discussed in Thread: C2000WARE Hi team,
In continuation to the previous thread i wish to ask two questions.
1) how to choose eroe band and settling time for the loop coffeficients calculations?
2) Why is the…
Part Number: TMS320F28388D Hello,
I'm tryting setting CLB TILES as the ECAP function.
I've refered and followed the example provided by TI, and been making my own PJT.
( CLB and ECAP Lab )
Input signal matching: Real external pulse signal…
Part Number: TMS320F28388D Other Parts Discussed in Thread: C2000WARE
Hello TI Team,
I am using a TMS320F28388D microcontroller with Code Composer Studio and C2000Ware 4.01.00.00 .
I am communicating with a MAX31856 through the SPI peripheral of…
Part Number: TMS320F28388D QUESTION: Why is the TMS320F28388D boot ROM not jumping to 0x80000?
PROBLEM DESCRIPTION:
I have GPIO72 and GPIO84 pulled high, which per Table 5-6 of the TRM (SPRUII0F page 716) should select "Flash / USB" mode. If I understand…
Part Number: TMS320F28388D Hello, We are having device emulating ABI interface connected to MCU TMS320F28388D. MCU is using eQEP module configured to measure position. We have problems with eQEP module initialization by Index input. Position is initialized…
Part Number: TMS320F28388D Other Parts Discussed in Thread: SYSCONFIG When I set up my clock tree for a 25MHz external oscillator and go into debug mode, the program hangs up on the following code:
#ifdef CPU1
//
// Verify the crystal frequency…
Part Number: TMS320F28388D hello,
is there a code sample for BISSC usage with encoder for the TMS320f28388d?
the only sampe that there is is for a differrent MCU...
Part Number: TMS320F28388D Other Parts Discussed in Thread: SYSCONFIG , C2000WARE Hi,
I am working with a TMS320F28388D and am trying to move MCANA from CPU1 to CPU2.
Observed Behavior
MCANA works correctly when configured and initialized from…