Part Number: TMS320F28P550SG Other Parts Discussed in Thread: C2000WARE-MOTORCONTROL-SDK , DRV8161 Tool/software: I’m planning to pair the TMS320F28P550SG with the DRV8353RS to build a sensorless BLDC motor controller. Does this seem like a good combination…
Part Number: TMS320F28P550SG Tool/software: Hi Champs,
When the LS8 LS9 RAM is configured as a CLA program, its address is 0x4000~0x7FFF, which conflicts with EPWM base address. After customer testing, it was found that using this LS8~9 memory would…
Part Number: TMS320F28P550SG Tool/software: My customer use F28P55 lanuchpad and connect to PC by USB port. Has set the S3 switch to be GPIO24=0, GPIO32=1; and set S2 switch to be IO28/29 to XDS.
The C2Prog program fail as below information, may we…
Part Number: TMS320F28P550SG Other Parts Discussed in Thread: TMS320F280049C , SYSCONFIG Tool/software: I am having a spurious PIE group 8 interrupt on the TMS320F28P550SG. When running under JTAG debug, the PIE Interrupt vector 88 is being triggered…
Part Number: TMS320F28P550SG Tool/software: Hi TI experts,
Two 28P55SG8 are used for SCI communication, and BUF data is read using a state query method. The SCI clock frequency is 150M/4=37.5M, the baud rate is 38400, the odd parity is enabled, and…
Part Number: TMS320F28P550SG Tool/software: Hi Team,
My customer is upgrade F28075 to F28P55, they have the same layout, use the same analog device, but F28P55 will damage(VDD short to GND) at 4KV surge, F28075 work well.
There are the test result…
Part Number: TMS320F28P550SG Tool/software: Hi Champs,
Customer now use own designed board and there is a JTAG error. When customer use CCS Target Configuration file to test the connection , it will show:
or
In order to reduce the PCB size…
Part Number: TMS320F28P550SG Tool/software: Hi All,
It says that underflow occurs when the position counter counts down after 0, but does this cause the CPU core to stop?
21.5.1 Position Counter Operating Modes
Best Regards,
Ito
Part Number: TMS320F28P550SG Other Parts Discussed in Thread: CCSTUDIO Tool/software: Hi,
I am trying to build a project with ccs
When i press `build` on the project it cleans it and then it's stuck without any message / output( see screenshot)…
Part Number: TMS320F28P550SG Tool/software: Hi champs,
I am asking this for our customer.
Is Bank4 (64KB) available on SG9?
From https://www.ti.com/lit/gpn/tms320f28p550sg (rev B)
It is available on
But it's not available on
Q:
Bank4…