Part Number: TMS320F28P650DH Tool/software: Hi Team,
There are two MCAN modules on F28P65, but I'm very confuse by below picture, so two MCANs use the same CAN core?
Best Regards,
Zane
Part Number: TMS320F28P650DH Tool/software: Hi
I can calculate one block CRC successfully and as I have understood from the documentation that incase of large memory we need to split it in <= 0xFFFF and the result becomes the seed of next block.
…
Part Number: TMS320F28P650DH Tool/software: Hi Guys,
Thanks in advance for your efforts to help me with the following issue
I want to use the DMA in the device tms320f28p650dh for the following transfers.
I have a source array of uint32 s_arr[8] and destination…
Part Number: TMS320F28P650DH Tool/software: Hi Expert,
My customer used to use BIOS as below, in BIOS, there is able to use SWI_POST function to change hardware interrupt to software interrupt, which will run after hardware interrupt like SCI interrupt…
Part Number: TMS320F28P650DH Tool/software: Hi Team,
Do we have fixed-point and floating-point computing performance comparison table?
My customer want to know the performance between two methods, thanks!
Best Regards,
Zane
Part Number: TMS320F28P650DH Tool/software: We found demo code. FPUmathTables : > FLASH_BANK0_SEC6 But without this definition, code still can be compiled pass.
Does this FPUmath Table have to be included in cmd file ?
Thank you.
Part Number: TMS320F28P650DH Tool/software: Hi champs,
I ask this for customer.
When using FreeRTOS, how to use FreeRTOS to control interrupts on C2000?
And in ARM devices, FreeRTOS cannot block interrupts with too high a priority. Does F28P65x have similar…
Part Number: TMS320F28P650DH Other Parts Discussed in Thread: ADS8588H , C2000WARE Tool/software: Hi Champs,
Customer now want to use TMS320f28P65x to retrieve from ADS8588H, it will need 2 SPI on F28P65x to received data from ADC8588H(DOUTA and DOUTB…
Part Number: TMS320F28P650DH Tool/software: Definition: Bank0, Bank1 is for CPU1, Bank4 is for CPU2.
Step1: DSP run, on this condition, CPU1 can operate bank1 R/W bank1. CPU2 can' see bank1.
Step2: Use register BANKMUXSEL to let CPU2 can access bank1…
Part Number: TMS320F28P650DH Tool/software: We are using TMS320F28P650DH.
There is strange behavior when use TBPHS to achieve phase shift function.
we take epwm_ex3_synchronization for reference.
EPWM1 create sync out pulse. EPWM2 sync in source is EPWM1…