Part Number: TMS320F28P650DH Tool/software: We use below code to operation flash. After run the flash program function. we can see the flash address have been written successfully. But we read the flash address. CPU2 run to dead status.
what's other…
Part Number: TMS320F28P650DH
Tool/software:
Team,
-I understand from the below thread that CPU2 is always independent from CPU1 (whether or not Lockstep on CPU2 is available on the specific variant). The lockstep feature is specifically between CPU2 and…
Part Number: TMS320F28P650DH
Tool/software:
Hi, can I use the internal ref/bandgap as reference for an external OpAmp? Is it the same for the F28P55?
Regards, Holger
Part Number: TMS320F28P650DH Tool/software: Hi Champs,
I see that peripherals can modify the assigned core via GPIO_setControllerCore(), and FLASH can modify the assigned core via SysCtl_allocateFlashBank. So after the peripherals and FLASH have been…
Part Number: TMS320F28P650DH Tool/software: Hi All,
Is it possible to use both single-ended and differential mode when using the F28P65x ADC? I am thinking of doing 6 single ended channels and 2 differential channels in an ADC interrupt. If I use single…
Part Number: TMS320F28P650DH Other Parts Discussed in Thread: PMP40988 , C2000WARE Tool/software: we are using TMS320F28P650 and want to run control DCL_runPI_L1 in CLA.
The clamath.h and CLA lib have been added. Check the include path, the path is included…
Part Number: TMS320F28P650DH Hi,
F28P65 CPU1 and CPU2's code, can they be updated from CPU1 at one time?
F28P65 5 flash banks. 3 are for CPU1 while the other two for CPU2. Can the CPU1 erase and write the 5 flash banks at one time, to do the CPU1…
Part Number: TMS320F28P650DH Other Parts Discussed in Thread: SYSCONFIG Hi Team,
Does the F28P65 support PTO? I download the newest SDK, but can't find F28P65 demo.
If support, how to port to F28P65?
Best Regards,
Zane
Part Number: TMS320F28P650DH Hi Team,
My customer want to compiler UL certification with use C2000.
we follow the coverage_test_instruction to coverage data files.
coverage_testing_instructions.pdf
But I am very confuse by set COVFILELIST, Why C2000 use…
Part Number: TMS320F28P650DH Hi Team,
Use VREG(internel LDO)(60℃) have high temperature than external LDO(40℃)
Will it improve with a different package? Such as use QFN to QFP?
Thanks a lot!
Best Regards,
Zane