Part Number: TMS320F28P650SK Tool/software: Hi,
When will the TMS320F28P650 data sheet with the single core devices in production state be released?
Regards
Richard
Part Number: TMS320F28P650SK Tool/software: Hi champs,
If we set ADCPPBxLIMIT to 4, means that we want to average four ADCPPBxRESULTs. Here are the questions,
Does PPB load ADCPPBxPSUM into ADCPPBxSUM only when ADCPPBxPCOUNT is equal to ADCPPBxLIMIT…
Part Number: TMS320F28P650SK Other Parts Discussed in Thread: PMP23338 , SYSCONFIG , C2000WARE Tool/software: Hi C2000 expert,
customer is asking some questions about CLA work in RAM.
Q1: customer is referring the PMP23338 demo code to develop a PFC. But…
Part Number: TMS320F28P650SK Tool/software: Hi,
We are looking for the latest generation MCU with 2x uPP support to interface with ADC and DAC (high sampling rate). Is it available?
Regards,
Ameenu
Part Number: TMS320F28P650SK Tool/software: Hi experts,
How will the power consumption of the F28P65 be, when running an EtherCAT slave and some simple IO-Operations ?
Kind regards,
Alex
Part Number: TMS320F28P650SK Tool/software: Hi,
From the TMS320F28P650 data sheet the best fit for our application is the single core part
TMS320F28P650SK6
However the data sheet states "Preview information (not Production Data)." for each of the single…
Luke,
The VCRC is reentrant provided you enable the corresponding option in the compiler.
--isr_save_vcu_regs is Blank by default, change it to ON.
Thanks,
Sira
Part Number: TMS320F28P650SK Other Parts Discussed in Thread: SYSCONFIG Hi champs,
When I use sysconfig tool to configure SDFM, there have no option to enable or disable SDFM internal input qualificaiton function. I build project and find that the SD_init…
Delaney Woodward said: Are you seeing any warnings (or outputs related to these functions) in the console when you build the project?
No, the compiler builds the project with 0 errors
Delaney Woodward said: Are you using the most recent version of the c28x…