Part Number: TMS320LF2406A Tool/software: Hi expert,
The driver of the TMS320LF2406APZ is abnormal, and the software cannot detect the burner.
The software used is BPWin5.8.0, and the software can only enter the DEMO mode if the burner cannot be retrieved…
Part Number: TMS320LF2406A Dear TI stuff,
I tried version 3.3.83.20, but it does not work. I got the error message “cannot run dspcl”. The following forum contribution deals about this error message:
https://e2e.ti.com/support/tools/code-composer…
Part Number: TMS320LF2406A Hi team,
I have a question from a customer that I believe you are better equipped to answer than me:
"I have some maintenance for an older TMS320FL2406A. We had purchased as CCS 3 way back when (from the ‘241 days!).…
Kailun,
It appears you were able to successfully establish connection with the target, which is very good. The fact that I see 0xFFFF in the first few locations of Flash tells me that the device is likely not secure. 0x40 is the beginning address of…
Part Number: TMS320LF2406A Hi Sir,
I would like to know where I can download the installer for SDFlash 1.63.00 or any other version can support for XDS510PP PLUS JTAG Emulator for LF2406.
Thank you.
Regards,
KC
Part Number: TMS320LF2406A Dear TI Team,
In addition, our customers also need to program TMS320LF2406A.
Kindly provide both programming specifications
Thanks in advance.
Best regards,
Austin
Part Number: TMS320LF2406A Hi C2000 team,
I know this is an older part, however, is there a recommended debugger and flasher for this device.
What is the best way to compile existing software on this device for windows 10?
Thanks!
Robert Kukis said: 1. Can the TMS320LF2406A DSP be programmed to count up to a number that would take 1ms to 2ms when the RS line / pin goes active [ low ] ?
No. Nothing can happen in the DSP until the -RS pin goes high.
Robert Kukis said: 2. Can the DSP…
Part Number: TMS320LF2406A Other Parts Discussed in Thread: TMS320LF2403A I have been interested in obtaining the BSDL files for JTAG programming of the Texas Instruments TMS320LF2406A and the TMS320LF2403A.
Initially, JTAG programming of these DSP/MCUs…
Part Number: TMS320LF2406A Hello,
I want tu use a Elpotronics Adapter (XStream-Iso for TI's C2000MCU) for programming a TMS320LF2406A.
So far we flashed the chip via JTAG.
With the new XStream-Iso we have to use SCI, because JTAG is not supported…