Part Number: TMS320VC5502 Hi team,
Will there be a functional problem with the TMS320VC5502PGF300 if there is a frequency deviation of 20MHz + 144ppm on the resonator connected to X1 (62-pin) and X2 (63-pin)? I checked P55 to P58 in the Data Manual, but…
Part Number: TMS320VC5502 Does CCS v12 or any of the v4.4.1 C55xx compiler or v5.42 DSP/BIOS have any utilities to show heap allocation/usage? I'm new to CCS and will be needing to verify that my C++ application's use of dynamic memory doesn't exceed…
Part Number: TMS320VC5502 How do I specify or find a csl5502.lib archive that supports the large memory model?
I'm importing a CCS v2.0 project into CCS v12.6
fatal error #16019: file "C:/ti/C55xxCSL/lib/csl5502.lib<csl.obj>" specifies…
Part Number: TMS320VC5502 I've imported a v2.0 project into Code Composer Studio v12.6 and after resolving several compiler errors, I'm ready to address linker issues.
After resolving library path issues for the BIOS and RTDX products, I have…
Part Number: TMS320VC5502 In my auto-generated maincfg.cmd linker command file, I have the following memory definition on line 190:
MEMORY { PAGE 0: DARAM: origin = 0x400, len = 0xcc00 PAGE 0: VECT: origin = 0x200, len = 0x100 PAGE 0: ExtPgm: origin …
Part Number: TMS320VC5502 I'm getting the following error when trying to connect the CCS v12.6 debugger to my target board.
Note: the XDS200 passes the JTAG Verify test.
Error connecting to the target:
(Error - 1063 @ 0x0) Device ID is not recognized…
Part Number: TMS320VC5502 Other Parts Discussed in Thread: SPRC133 I'm working to setup a build environment in Code Composer Studio v12.5 for the TMS320VC5502 and then importing a v2.0 project into the v12.5 environment.
During custom installation…
Part Number: TMS320VC5502 The following linker directive gives a warning -- #10068-D: no matching section.
Which library module or component contains a .clk section?
/* MODULE CLK */ SECTIONS { .clk: block(0x20000), RUN_START(CLK_A_TABBEGb) { CLK_F_gethtime…
Part Number: TMS320VC5502 Using CCS v12.6; I have legacy C++ code that uses the #pragma DATA_SECTION directive to create a custom section name
e.g.
#pragma DATA_SECTION ("DMABuffers"); Int16 gScratch[NCISFRAMELENGTH];
Which is producing the following…
Part Number: TMS320VC5502 Hello everyone, when I press the "debug" button, I experience a freeze, followed by error -2172 as mentioned in the title.
I am using a custom DSP board equipped with a C5502.
I am using an XDS200 debug probe.
…