Part Number: TMS3705 Other Parts Discussed in Thread: TMS37145 , , UCC27424
Hello, We are trying to detect the Transponder TMS37145 using the Basestation IC TMS3705FDRQ1. The Coil used here is having Inductance of 300uH. After the charge phase, we are…
Part Number: TMS3705
Hello Team,
We are using the TMS3705 and encountered communication failures during IEC 61000-4-6 conducted immunity testing.
After adding a common-mode choke (BNX028-01) to the antenna communication path, immunity performance…
Part Number: TMS3705 Hi,
I am seeing severe waveform distortion after R36 in my TMS3705 receiver circuit:
* Frequency: approximately 134 kHz * Before R36: roughly sinusoidal, peak-to-peak ~0.74 V * After R36: distorted, peak-to-peak ~1.39 V, with…
Part Number: TMS3705 Other Parts Discussed in Thread: UCC27524 Dear TI Experts, I am using the TMS3705 for reading ISO 11785 HDX tags. The schematic is based on the standard TMS3705 HDX reference design, but the reader is not able to successfully read…
Part Number: TMS3705 Tool/software: Team,
My customer developed a prototype with TMS3705 and conducted an actual measurement evaluation of the antenna current. There was a large discrepancy between the current value calculated based on the assumption…
Part Number: TMS3705 Hello,
I am looking for solution for Keyfob detection using Tranponder tag in Keyfob and base station IC using below solution
The Measurement or tansponder detection distance requirment is 3-5cm.
Base station IC :- TMS3705FDRQ1…
Part Number: TMS3705 Tool/software: Hello! I hope this message finds you well.
We are currently facing a technical issue in a project and would like to request your support, in case you have dealt with a similar situation with any customer.
We have…
Part Number: TMS3705 Other Parts Discussed in Thread: TRPWS21GTEA Hello TI team,
Our customer asked us about the combination of TMS3705GDRQ1 with TMS37145TEAIES.
1, Is it possible to use this combination if no issue by customer's evaluation?
2,…
Part Number: TMS3705 Other Parts Discussed in Thread: TMS37145 We design and develop equipment related to access control systems.
We are considering developing your transponder, which we received a request from a user to use as an authentication device…