Other Parts Discussed in Thread: TMS570LS2125 , HALCOGEN Hello,
I have a question for "Table 5-10. MibADC Operating Characteristics Over Full Ranges of Recommended Operating Conditions" described in page 121 of data sheet of TMS570LS2125 (spns164).…
Gareth,
We have integrated the initialization code generation into HALCoGen and therefore, removed the previously posted code from the app note/zip file to avoid confusion. HALCoGen now gives you the options of enabling/disabling most of the tests that…
Well, It appears that the issue is still there. The error I get falls into EEPROM bank ECC:
CortexR4: Error during Flash verification (Flash algorithm returned error condition). Operation cancelled. CortexR4: Flash verification returned error condition…
Other Parts Discussed in Thread: TMS570LS2125 Sirs,
On the page-120 of the TMS570LS2125 DS "SPNS164" we find the MibADC input equivalent circuit as Fig 5-1.
In the figure we find Cmux and Csamp.
Then, can I ask the initial voltage of the caps…
I ran in to a situation today where the watchdog RTIDWDKEY register was being written to before the watchdog was configured an enabled.
Even though the correct patterns were written in the correct order, the processor was being reset on the write of…
Other Parts Discussed in Thread: TMS570LS2125 Hello,
I am working with a TMS570LS2125 and I want some sectors of flash memory to be protected from erasure and overwrite.
Can you please tell me where I can find the detailed information on how to protect…
Hi,
Additional symptoms are that CoreSight debug port (DP) is responsive with nRST line low (I can read and write CTRL/STAT register) but accessing ROM table to detect Cortex debug components fails. Same procedure works with TMS570LS2136, TMS570LS2125…
Other Parts Discussed in Thread: UNIFLASH , TMS570LS2125 Hello ,
i just installed uniflash 3.1 and did "updates". prior i used 3.0
with 3.0 i never got an error messages while programming tms570ls2125
now after installing 3.1 and using the same…
Other Parts Discussed in Thread: TMS570LS2125 Hello,
My TMS570LS2125 ADC input pin will have voltage from -1V to +3V. The voltage -1V exceeds the absolute maximum ratings, -0.3V.
To protect the ADC input pin from the -1V, The ADC pin current should be within…