Part Number: TMS570LS3134 Hi, I have a question from my customer regarding below TRM description. At section 24.17.8 Auto-Bus-On Time Register (DCAN ABOTR) in SPNU499B, there is a NOTE saying; On write access to the CAN Control register while Auto-Bus…
Part Number: TMS570LS3134 Other Parts Discussed in Thread: TMS320F28335 , , TMS570LC4357 Hello,
one of my customers is asking about the performance of the TMS570LS3134 compared to the TMS320F28335.
On their current project they are using the TMS320F28335…
Part Number: TMS570LS3134 hi,
as the title, is there any PC GUI can play as the host side to handle the TMS570 bootloader?
any I/F is ok, like UART,I2C,SPI...etc.
Erik
Hello Nolan,
I believe the SW you are referring to is the Hercules MCU Safety Demo SW. It should be included in the kit on the CD but it would probably be an older version. The latest version can be downloaded at this link: www.ti.com/.../hercules_s…
Part Number: TMS570LS3134 Other Parts Discussed in Thread: TMS570LS20216 Hello there,
In our upcoming project design we need to sample at 100 MHz two separate square input signals of between 7 kHz and 12 kHz, and to provide the free-running counters (10…
Part Number: TMS570LS3134 Other Parts Discussed in Thread: HALCOGEN Hi everybody,
I'm facing problems working with TMDS570LS31 HDK (in fact same Problems with two boards...) and things seem to get worse day by day:
After powerup, the uC sometimes doesn…
Part Number: TMS570LC4357 Other Parts Discussed in Thread: TMS570LS3137 , TMS570LS0714-S , TMS570LS3134 , TMS570LS1227 Provide the list of documentation bugs in Hercules devices (TMS570Lx, RM57Lx, RM46Lx, RM48Lx etc).
Part Number: TMS570LS3134
I am wondering if it is possible to emulate a video port with the N2HET. Therefore N2HET would need to generate the following signals:
PCLK (pixel clock) ~ 20 MHz, basically a PWM, 50% duty cycle.
VOUT_D0 to VOUT_D7 (video parallel…
Part Number: TMS570LS3134 Hello, I got two questions from customer regarding Errata ADC#1. 1) The workaround#2 says “Configure the two ADC modules such that their sampling periods do not overlap”. Is there any timing gap required between…