Part Number: TMUX1108 Hi Team,
Please help to check what's wrong with it?
My customer schematic is below and while the TMUX1108 is disabled, they can see the 2uA with a current meter.
All the channels of S1 to S1 are with the same problem.
Pls help…
Hello zeming,
Sorry for misunderstanding your initial question.
To better understand your question I just want to clarify some things
Uart is a 2 wire communication protocol where devices can communicate with each other over 2 wires which are the TX…
Part Number: TMUX1108 Other Parts Discussed in Thread: LMG1020 , Hi ti
I designed a circuit: use 1pcs LMG1020 + 1pcs TMUX1108 + 8pcs MOSFET, Testing found that TMUX switch pins are often burnt out;
The output of LMG1020 is a pulse current, with a peak…
Part Number: TMUX1108 Other Parts Discussed in Thread: XTR111 , TMUX1119 , TS5A12301E , TS5A4624 , TS5A6542 Hello Team, I want to design a system using TMUX1108. I have a connector terminal with an analog voltage (0-10V) or current (4-20mA) as a sensor output…
Part Number: TMUX1108 Hi TI
The customer uses this chip, which is powered by 5.3V, and the address pin level is normally controlled by 3.3V. Six pieces have been welded, and one piece has a short circuit between A0 and GND. Please help to analyze the…
Part Number: TMUX1108 Other Parts Discussed in Thread: LM4120 Hi,
I have a 128Ch Mux (16x TMUX1108 parallel) system where I use LM4120 1.8V as single supply to VDD of all TMUX1108. VSS are grounded. EN pins of TMUX1108 are also at 1.8V. Each TMUX1108…
Part Number: TMUX1108 Hi Experts,
Our customer is looking for a SPICE Simulation model for TMUX1108. We know that the IBIS model is the only available on TI.com. We just wanted to check if we now have a SPICE model that we can share with our customers…
Hey Deepak, Well the idea here would be to use muxes on both sides to try and isolate and reduce the loads on both sides of the amp. Basically you could use 4 TMUX1108 where the 8 signals would have an associate TIA. Then from there you would mux those…