Part Number: TMUX1136 Hi,TI expert:
Is the chip silk-screened in the following image corresponding to the TMUX1136 chip? Please confirm . Thank you!
TI27 P14RA 1136
Part Number: TMUX1136 Tool/software: Hi
I thought the control notations in the datasheet Table 7-1 and the schematic were different, which is correct?
Thanks,
Part Number: TMUX1136 Other Parts Discussed in Thread: TMS3705 , TMUX1104 , TS5A3159 , LMS4684 Hello,
I am currently designing an RFID dual system using TMS3705 and HTRC11001T. Their antenna outputs are selected via an analog switch and routed to the…
Part Number: TMUX1136 Tool/software: Hi Team,
Use TMUX1136 to implement CAN bus switch switching function for switching access to different BMS. For example, connect or disconnect BMS10_CAN to BMS-CAN. Recently, it has been found that there are chip…
Part Number: TMUX1219 Other Parts Discussed in Thread: TMUX1136 Tool/software: Hi,
TMUX1136 is 2CH 2:1 SPDT, TMUX1219 is 1CH 2:1 SPDT, If we want using 2* TMUX1219 to replace 1 *TMUX1136, is there anything need notice?
Thanks!
Jeff
Part Number: TMUX1136 Can I switch 2 BUSes using the TMUX1136 analog 2x DPDT and use a single output PCB connector? - 1 CAN(5V) with TCAN 1042 [1a/1b] ; - 1 RS485 with SP485EN-L/TR [2a / 2b] ; - D1 and D2 out to the connector? Channel accuracy can cause…
Part Number: TMUX1136 Tool/software: Need clarification for the below item ASAP as production has been stopped due to below issue. Need your support ASAP.
Supplier: Mouser
Make: Texas Instrument
As pe the Texas Instrument data sheet, the body marking…
Part Number: TMUX1136 Other Parts Discussed in Thread: TMUX1574 Hi
This TMUX1136DGSR, does the customer want digital? Analog is more expensive
The requirement is 2:1 2 groups or 2:1 4 groups VCC 3.3V The customer's application is to switch SPI 4 wire…
Part Number: LDC1614 Other Parts Discussed in Thread: TMUX1136 We are working on an application that identifies inductances in the order of ~200nH, With series resistances of ~0.5Ohm.
Due to the relatively low quality factor we need to use the LDC1614…