Part Number: TMUX1209 Other Parts Discussed in Thread: INA827 , ADS1261 , , TMUX1109 Tool/software: Hi,
I have designed a schematic for an analog measurement as shown below. On the analog input side, I can also receive negative analog signals from some…
Part Number: TMUX1109 Other Parts Discussed in Thread: TMUX1209 Hi,
I have a PCB designed for TMUX1209PWR, but it is currently "out of stock" at pretty much any distributor I could find. According to the website TMUX1109 is a "drop-in replacement" for…
Part Number: TMUX1209 Hi,
I want to calculate 16-bit settling time of the MUX when channels are switched. The datasheet specifies settling time of 33ns for VDD =5V. The definition of settling time is given as "Transition time is defined as the time taken…
Part Number: TMUX1209 Hello expert, My customer is evaluating TMUX1209. Then, they observed100mV as high impedance on DA/DB during EN=0. I guess it is from internal protection diode or something but there isn't any explanation regarding this on datasheet…
Part Number: TMUX1209 Other Parts Discussed in Thread: TMP107 We have a 2 * 1:16 multiplexer device, which communicates with sensors and reads battery voltages. When measuring the batteries, we have an in-line resistor to protect from over current draw…
Part Number: TMUX1209 Other Parts Discussed in Thread: ADS1118 , , TMUX1109 Hello, We plan to use two chips of TMUX1209 together with ADS1118 to connect eight thermocouplers. Each channel of ADS1118 connect to one TMUX1209 which connect four thermocouplers…
Part Number: TMUX1209 Hey,
when selecting a MUX for a UART. What parameters should I consider? In this case, What MUX can I use for a UART to connect to 3 slaves? Will a TMUX1209 work?
Part Number: TMUX1209 Other Parts Discussed in Thread: TMUX1204 , Hi all
My customer has preselected the TMUX1209 and the TMUX1204 because of the 1.8V logic compatible control inputs.
In their system the uC supply is -2V / 0V while the analog supply for…