Part Number: TMUX1308A In a 6-year-old forum post , the user asked if it was possible to connect two 8:1 multiplexers by tying their Ax and Ex pins together. I assume this was an old notation for the part because the modern datasheet doesn’t list Ax and…
Part Number: TMUX1308-Q1 Tool/software: Hi team,
Our customer has some questions about injection current control in TMUX1308-Q1. They want to understand this function can work to protect Source pin when it is short to 12V battery.
(Expected use case…
Part Number: TMUX1308-Q1 Hi, Support Team
TMUX1308-Q1 about A0, A1,A2 pin could connect to I/O voltage 3.3 of MCU?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TMUX1308-Q1 Tool/software: Hello,
I was trying to calculate the FIT rate for this component using the ISO26262 standard. I have formulated a calculation where, given a FIT from the supplier using the ISO26262 standard and an standard mission…
Part Number: TMUX1308-Q1
Tool/software:
Hi Experts, '
Is there any guidelines to follow regarding the input when the TMUX is not powered.
Can i apply input voltage when the supply is not available.
Thank you for the guidance.
Regards,
S…
Part Number: TMUX1308-Q1 Tool/software: Hi
I have added a image of the datasheet, which I would like to know when all the pin is on what will be the injection current and also the value of clamping voltage
Thanks
Part Number: TMUX1308-Q1
Tool/software:
Dear MUX experts,
my customer is using TMUX1308-Q1 in one of his designs.
Now we have a question about the effect of the injection control on the input signal.
Our circuit looks similar to the one in…
Part Number: TMUX1308-Q1 We need some mandatory informations about it:
Chip Category;
End of production (EOL);
Technology;
Node Size;
Wafer Size;
LeadTime for Alternative;
Wafer Fab: Supplier, location, share and readiness SOP;
Assembly…
Part Number: TMUX1308-Q1 Hi team,
I have a question. Can this device source/sing current? If yes, how much current can this source/sink?
Best Regards,
Shoji