Hi Tommy,
I agree with Clemens on this. The Tmux136 is characterized by Ron vs voltage input so there is no curve like the one you provided. However the mux can be modeled as a resistor and the solution Clemens described is applicable.
Thanks and Regards…
Part Number: TMUX136 Other Parts Discussed in Thread: TMUX154E , TS5A9411 Hi, would like to know at which frequency the charge pump runs and are there any spectrum plots available showing what kind of spurs it creates. Asking as considering if this can…
Part Number: TMUX136 Hi Expert,
I saw this device no need external pull up resistor for design, but I still would to double check with you for below question:
If customer send signal from COM1/2 to A/B port, does it need pull up resistor on COM1/2 ?
if…
Part Number: TMUX136 Other Parts Discussed in Thread: TS3DV642 Hi Team,
Our customer would like to confirm if the TMUX136 can be used as Mux/Demux for MIPI signals w/ frequency of up to 720 Mbps/lane or up to 1.6Gbps/lane. If not, do we have a mux that…
Part Number: TMUX136 I HAVE RELATED QUESTION REGARDING SWITCHING OF ANALOG (CVBS) & DIGITAL (3G-SDI) Video signal upto 2 channel max. I have 2 HD-BNC Connector on board wherein either CVBS (PAL) or SD/HD/3G-SDI video source may be connected. If it is…
Part Number: TMUX136 Hi team,
I would like to ask about maximum stub length in TMUX136.
The datasheet suggest the stub length to be designed less than 200mm, but in 6GHz application scenarios the signal wave length is just 24mm.
I wonder if the 200mm…
Part Number: TMUX136 MPN : TMUX136RSER and TMUX136 M RSER
these two parts share same datasheet , their function is the same , but I can't know what different between them e xcept for " Device Marking"
need your help on this part.
Part Number: TMUX136 Other Parts Discussed in Thread: TMUX154E , , SN74CB3T3257 Hi Expert,
Customer would like to check does TI has solution for I3C HUB /I3C MUX / I3C level shift?
And could it support I3C high voltage(3.3V)?
Regards,
Mark