Part Number: TMUX136 Hello,
Regarding to EN on TMUX136, my customer is asking a question.
(Question)
・When EN is always enable ,is there any problem on device?
For example, is there any problem at following condition?
1) After EN is enable, TMUX136 power…
Part Number: TMUX136 Hi dear supporting team,
customer want to use TMUX136 to switch BTW CML & LVPECL level the detail as below:
1. input to port1.
2. when the input is 10Gsps CML signal, output from port1 without any matching.
3. when the input…
Part Number: TMUX136 Can the TMUX136 be used to route CML signals? I have two ChannelLink II transmitters and I would like to use the TMUX136 to route these to a single ChannelLink II receiver.
Part Number: TMUX136 Hi Team,
The CAD file (.bxl) available for TMUX136 is pin mismatch vs the datasheet. The COM1 and COM2 on the .bxl file are swapped.
Can you check this one? We assumed the datasheet is safe to follow.
Regards,
Renan
Part Number: TMUX136 Other Parts Discussed in Thread: TMUX1136 Hello,
Can you confirm if the TMUX136 is a make-before-break switch or break-before-make switch. I was not able to verify this in the datasheet. Or if this does not matter for I2C switching…
Part Number: TMUX136 e2e,
Regarding TMUX136, customer would like to know what’s the Recommend Operation Temperature and Recommend Junction Temperature?
Part Number: TMUX136 Other Parts Discussed in Thread: HD3SS3202 , Hi there,
My customer has a similar application as below link, but they just use TMUX136 to switch 1.25Gbps LVPECL. 10G CML is switched by HD3SS3202. Here are two questions for TMUX136.
1…
Hi Rudy,
The difference for this can be found in the datasheet Tape and Reel information.
The devices have different tape and reel dimensions and the Pin 1 quadrant is in a different location.
Part Number: TMUX136 Other Parts Discussed in Thread: TS5A23160
Hi TI Team,
Can you please provide the best TI solution to Maxim MAX20336.
P2P is nice to have but not a must.
Thank you,
Liz