Part Number: TMUX1511
Hi Everybody,
I was looking for a small 2:1 mux for HD-SDI/SD-SDI (Not 3G) video signals and came across some old threads on E2E e.g: HD-SDI & CVBS signal switch and SDI Signal multiplexing
If I am not mistaken TMUX1511 looks…
Part Number: TMUX1511 hellow
I would like to know the change of 10℃ interval of TMUX1511 (DVDD = 3.3V -40~125℃). Datasheet from Ttransition VS Temperature is present in Datasheet, but the Temperature impact of Ton/Toff could not be verified. Best Regards…
Part Number: TMUX1511 hi,
Fout2 inputs a frequency square wave from 10KHZ to 100KHZ, and SEL1 and SEL2 are both high or low levels. SEL3 and SEL4, due to the connection of inverters, have opposite levels to SEL1 and SEL2. When SEL1 and SEL2 are high,…
Part Number: TMUX1511 hi,
When Fout2 connects signals from 10KHZ to 100KHZ, the measured TP10 and TP11 are a set of reverse frequency signals. A 1pf capacitor is welded at the position of C31, and the voltage TP13 0.0024V TP15 0.0015V TP16 0.0015V TP17…
Part Number: TMUX1511 Other Parts Discussed in Thread: TMUX2889 , TMUX4827 , TS5A22362 , LM7705 Hi TIer
1. Could TMUX1511 transmit negative voltage? (When use single ended power supply)
2. When customer use 5V power supply , The channel generates a 7V pulse…
Part Number: TMUX1511 Other Parts Discussed in Thread: TMUX6111 Based on below application, if the output short to 16V, can the tmux1511 be protected without the diode.
Assume there is body diode inside the input of tmux1511, and current is limited by…
Part Number: TMUX1511 Other Parts Discussed in Thread: TMUX1111 Hello TI support.,
We intend to use TMUX1511 in battery powered application where we think of below use case,
Application
We shall be using TMUX1511 between uC & peripheral interfaces like…