Part Number: TMUX1574 Tool/software: Can I use two TMUX1574 back-to-back to switch between two Sources (Xilinx POD & Boundary Scan) and switch to Two Destinations as shown below?
Hello Syed,
The TMUX1574 is a passive device that doesn't actual drive any signal on it's own. It only passes the I/O signal through, depending on the logic. So there isn't any VIL, VIH, VOL or VOH for these pins. They are just analog I/O's.…
Part Number: TMUX1574 Tool/software: Dear Ti
Is the TMUX1574 suited for differential signals like SGMII ?
From the datasheet it seems to be only applicable to single-ended applications?
Regards
Piet
Part Number: TMUX1574 Tool/software: Hi,
We are using TMUX1574 MUX for QSPI Flash memory. Our application is bidirectional purpose (Read and write) operations on flash memory.
Related to MUX we have few queries:
In MUX datasheet only VIL,VIH is given…
Part Number: TMUX1574 Tool/software: Hi,
Which would be the reference design closest to TMUX1574 with SPI muxing?
I would like to get the schematics of the same.
Thanks
Nandini
Part Number: TMUX1574 Other Parts Discussed in Thread: TMUX646 , TMUX121 , TMUX136 , TMUX131 Tool/software: Looking for 1:2 SPDT Analog MUX for RMII/NC-SI (7 signals, 100Mbps) so 8Ch would be fine.
Thought of using 2 Qty of TMUX1574 ( 4ch SPDT).
Recommend…
Part Number: TMUX1574 Tool/software: Hi team, we are using TMUX1574RSVR in our project. we are facing issue when we transmit SPI signals through that part. Issue: we are transmitting SPI signals with clock frequency of 125khz with the voltage level as 5V…