Part Number: TMUX1574 Hi Team,
Quick question, in the TMUX1574 truth table, when the EN/ is a value of 1, is the S side completely disconnected from the D side? Or is it possible that if a signal is applied the to D side, it could travel through a body…
Part Number: TMUX1574 We have a few concerns about Vdd=0v.
1. Vdd=0v, how about IO pin is Hi-Z or something
2. Vdd=0v, how about the logic pin
our application is SPI tree.
When the Vdd is no power supply, we need measure the IO is Hi-Z, not IO connect…
Part Number: TMUX1574 Hi Team,
Is there a negative consequence or latch up condition that could occur is voltage is applied to EN/SEL pins before VDD has power?
Thanks,
Jared
Part Number: TMUX1574 HI,
Parts like TMUX1574, tend to only only list the typical propagation delay in the data sheet.. How should i determine the max propagation delay? Is it listed elsewhere or should I derive it from another specification? Please explain…
Part Number: TS3A27518E Other Parts Discussed in Thread: TMUX1574 , Hi Team,
I found there is a huge gap between the price of these two parts. Could you advise me on that and itemize the differences, except for the channel numbers (a and 6)? My client is…
Part Number: TMUX1574 Other Parts Discussed in Thread: TMUX1309 Hi sirs,
My customer designed TMUX1574 for 1 to 2 channels SPI switch. Now she wants to find a switch of 1 to 4 channels SPI to reduce component counts. Does TI have 1:4 SPI swittch?
Part Number: TMUX1574 Hi team,
Is the default condition of pin 9 and pin 12, which refer to D3 and D4, high impedance when these pins are not connected?
Best regards,
Wendy
Part Number: TMUX1574 Hi team,
Customer hopes to use it output analog sine wave.
Input would be 1Vpp(S1) and 3Vpp(S2) 100kHz sine wave.
They need the output be totally the same as S1 or S2.
Could TMUX1574 support this function?
If not, which part do you…