Part Number: TMUX1574
I'm considering using TMUX1574 to switch between two sim cards just like the illustration posted below. The GSM modem provides power to the SIM_VCC so both sim connectors will always be powered even when the mux is switched off…
Part Number: TMUX1574 Dear Texas Team,
I've referenced the "7.5 Electrical Characteristics" section of the datasheet for the Switch with 1.8 V Logic "TMUX1574DYYR" and found that it specifies a maximum High Level Input Voltage (VIH) of 5.5V. However,…
Part Number: TMUX1574 According to the TMUX1574 data sheet, the Vih (Input logic high) is between 1.2 to 5.5V.
I have a SPDT switch connected to the SEL pin that switches between 0 to 1.2V, would the TMUX1574 work reliably?
The 1.8V logic I/O supposed has…
Part Number: TMUX1574 Other Parts Discussed in Thread: SN74LV4052A I have been looking at analog muxes 2:1 and 4:1 for some time, the TMUX1574 finally came up as what seems the perfect choice for 2:1: low capacitance, low leakage, ultra small package…
Part Number: TMUX1574 Other Parts Discussed in Thread: TMUX646 , TS3A27518E Hi there,
The picture below shows an application of the TMUX1574 for a Quad-SPI.
According to the datasheets of the MUX and the Quad-SPI, it seems 2 MUXs can work together.
Setup…
Part Number: TMUX1574 Hi team,
Customer would like to use TMUX1574 as a mux for 2 slave device, do they need to get pull up resistor as both side of TMUX1574?
Thanks and Best Regards,
Will
Part Number: TMUX1574 Hi,
Do you think TMUX1574 is good fit this application? Thank you.
Default Master1 turns on to connect slave SPI ROM and the SPI Mux switch to Master2 when Master2 set the GPIO to control the Mux.
Speed 40MHz
SCLK : Serial Clock…
Part Number: TMUX1574 Hi Team,
I have a question about the Spice model of TMUX1574.
I am simulating TMUX1574 with PSpice for TI. When VDD voltage = 5V, it works as per the datasheet, but when VDD voltage = 3.3V, it doesn't work. (Input signal is not…
Part Number: TMUX1574 Other Parts Discussed in Thread: TS5A22362 , TS5A23159 Dear team,
We have an application, and input signal range is -2.5V~2.5V(square waveform).
If VDD connect to 3.3V, Is negative input signal acceptable?
If not, did we have mux…
Part Number: TMUX1574 Dear team,
Does TMUX1574 support I3C/ 3.3V level?
I find a FAQ below, and based on the post, TMUX1574 should be good for I3C/ 3.3V application.
https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches…