Part Number: TMUX1575 Dear TI Support,
I'm designing a new board with your TMUX1575 chip.
In the datasheet there is a layout example, but I need further information. Is possible to have an in depth description of the rounting, vias and PAD of the…
Part Number: TMUX1575 Other Parts Discussed in Thread: TMUX1511 , Hi all,
I have a customer using the TMUX1511 to implement a SPI flash sharing scheme. There are 2 "master" devices that need access to the same SPI flash device, but not simultaneously.…
Part Number: TMUX1575 Is there any problem in the Float state for unused ports?
If we need measures against external noise, could you be able to show me the recommended circuit?
Thank you in advance for your help.
Part Number: TMUX1575 Dear team
Does TI have such an analog switch?
The system defaults to the slave clk path, which can be switched when the analog switch detects that the master clk has a signal.
When the analog switch detects that the master clk has…
Part Number: TMUX1575 Hi,
Customer is looking for the IBIS or S-parameter model of TMUX1575 for their SI analysis. Can you please provide to us?
Thank you in advance.
Regards, Maynard
Part Number: TMUX1575 Hello, My customer would like to make EN always active.
Can they just short EN to connect to VDD?
Or should they put a resistor, for example 10Kohms, between EN and VDD? Best regards, K.Hirano
Part Number: TMUX1575 Hi,
I want to use TMUX1575 for a DUAL SIM/DUAL Modem application.
So far I used ONSemi's FXLA2203UMX which have a full flexibility. Unfortunately it become obsolete and I am looking for an alternative.
1. Can TI's TMUX1575 support…
Part Number: TMUX1575 Hello,
My customer would like to have either IBIS model or s-parameter of TMUX1575.
Can TI provide either one of them?
Best regards,
K.Hirano
Part Number: TMUX1575 Hello,
My customer plans to use TMUX1575YCJR and are reading the datasheet.
However, a package drawing is missing.
Could you provide WCSP (16) 1.34 mm × 1.34 mm package drawing, please?
Best regards,
K.Hirano
Part Number: TMUX1575 Other Parts Discussed in Thread: SN74CBT3245A , SN74CBT3245C , SN74CBT3861 , SN74CBTLV3861 , SN74CBT3257C , TMUX1574 , , SN74LV4066A , TMUX1511 , TS5A23157 , TMUX1072
System isolation is critical for power sequencing, managing bus contentions…