Part Number: TMUX2889 Hi,
I have some doubts about the frequency operation of this component.
Does this maximum signal swing graph means that if I apply a signal between 0 and 3.3 V at Sx, it won't work okay beyond 50 kHz?
If this is the case…
Part Number: TMUX2889
Dear TI
I am seunghyeon Yun in charge of RF part.
I need a circuit configuration for a new device as below picture.
I need a positive/negative voltage to operate the load device like aa H-bridge.
Are there recommended parts…
Part Number: TMUX2889 previously E2E post
https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/1256852/ts5a22362-inquiry-regarding-ts5a22362-ic-characteristics-and-alternatives?tisearch=e2e-quicksearch&keymatch…
Part Number: TMUX2889 Other Parts Discussed in Thread: TMUX4827 , TMUX6236 Can "TMUX2889" swith the input signal of 125kHz/10Vpp sinusoidal wave?
There are below description in the data sheet. - Signal path input/output voltage is -5.5V min and +5V…
Other Parts Discussed in Thread: TMUX2889 , TS5A23160 , TMUX1072 , DRV2605 , TS5A26542 , TMUX6234 part number: TMUX2889
Hi TI,
In the TMUX2889 datasheet page. 10 - Figure 6-14. Insertion loss versus frequency,
We can see there is no insertion loss…
Part Number: TAD5212 Other Parts Discussed in Thread: TMUX2889 , Is there an application note describing the short circuit detection?
The situation of interest is a stereo singled-ended capacitor (270uF) coupled output connected through a TMUX2889 to…
Part Number: TMUX4051 Other Parts Discussed in Thread: TS5A22364 , TMUX2889 Hi, I have an application involving audio signals and would appreciate your help in verifying the following: Can the TMUX4051 IC be used to switch audio signals? Are there any…
Part Number: TMUX1119 Other Parts Discussed in Thread: TMUX2889 , TMUX2819 , TMUX4827
hello,
Does it suppport DC on its input?
Can it be used with negative inputs (specifically 0 to -5V)?
If not, can you suggest a SPDT that supports 0 to -5V inputs…
Part Number: TMUX4827 Other Parts Discussed in Thread: TMUX2889 , Hi team,
My customer would like to know detail information of package outline. But the datasheet doesn't include package outline information.
While, TMUX2889 seems use same package…