Part Number: TMUX6202 Hi, because of PIN 2 and PIN 5 are not internally connected, we want to put the same potential on it. Is their any reason to avoid this? In detail, we wand wo put on PIN 2 the same potential as on PIN 1 (so this two pins are shorted…
Part Number: TMUX6202 Other Parts Discussed in Thread: TMUX6201 Tool/software: Hi Expert,
My customer is using TMUX6202, but find there is a update for truth table between 2023 and 2024 version. so please help to check.
our device also follow…
Part Number: TMUX6202 In my design, I need to switch a 68 ohm termination on and off. the bus voltage is 22Vpp. Can I use TMUX6202 for this? Please see attached picture.
Thanks!
Yossy Goldenberg
Part Number: TMUX6201 Other Parts Discussed in Thread: TMUX6202 Tool/software: I build a design with many many TMUX6201. Following the datasheet, I inotialized most of them with SEL=0 to turn off. As I was debugginh it turned out that SEL was active LOW…
Part Number: TS3L501E Other Parts Discussed in Thread: TMUX4053 , TPS1H000-Q1 , TMUX6202 , TMUX6201 Tool/software: TS3L501ERUAR I am using this part number device as the ethernet switch over circuit. can you please suggest the part number for analog and…
Part Number: CD4052B Other Parts Discussed in Thread: TMUX6202 , SN74LV4052A , TMUX1309 Hi
Do Con and Coff change with Vs/Vd input/output voltages? In the customer's system, the CD4052B is connected in front of the ADC. Only when the MUX input voltage…
Part Number: TMUX7412F Other Parts Discussed in Thread: TMUX7412 , TMUX6212 , TMUX6202 , , TMUX6201 Dear TI Engineer:
We have purchased some products from your company and encountered two issues during use, which are inconsistent with the manual description…
The following table helps select th e right multiplexer and switch with Mid Voltage 25V =< VSIGNAL =< 99V in different configurations:
Precision , Protection , Automotive , Extended Temperature
Configuration
16:1…