Part Number: TMUX6208 Can you please help me to confirm the solder profiles recommended for this component MPN: TMUX6208RUMR
Maximum Reflow Temperature (°C)?
Reflow Solder Time (Sec)?
Number of Reflow Cycle?
Part Number: TMUX6208 The TMUX6208PWR test revealed that when a load is connected at the D terminal, S acts as the power supply. When the D terminal is connected to an electronic load (20mA), the conduction time of S and D significantly increases to 1…
Part Number: TMUX6208
Tool/software:
I'm currently testing TMUX6208 on a breadboard and have connected the TMUX6208 chip with the following 5V and GND shown in the figure below.
I want to be able to measure the 5V (given on the D pin) on whichever…
Part Number: TMUX6208 Tool/software: TMUX6208 has a bad channel, and the impedance of the channel to the ground is 28Ω. If the Sx port is powered on before a single chip is powered on, will the chip fail?
Part Number: TMUX6208 Hi,
I have connected the signle ended analog input signals (0-5V) to the Source pins of TMUX6208. So, I have provided 5V to VDD pin of the IC and VSS is directly tied to GND. Is it fine?
Or Shall I need to connect VSS pin to…
Part Number: TMUX6208 Hi team,
I would like to know the EN,A0,A1,A2 Vth what voltage is.
Base on datasheet. If over 1.3V will be high level is correct? but max is 36V.
As I know the voltage of EN pin is usually not too high.
Part Number: TMUX6208
Hi,
I have 21 V AC (Maximum) Signal in my system. I have used a resistor deivider to reduce the voltage to 3 V AC as my Input VDD voltage to TMUX6208 is 3.3V DC. VSS is connected to -3.3V DC.
Can I feed 3V AC signal to Any…
Part Number: TMUX6208 Hi Expert,
We need you help for our customer's application.
They are currently developing some kind of measurement electronics.. The basic idea is the following: They would like to take a high precision ADC. They would like…
Part Number: TMUX6208 Other Parts Discussed in Thread: TMUX7462F , TMUX7308F Hi,
I have a design with 24 TMUX6208 multiplexers on the same 28V power rail. some of them sharing the output connections on the connector and the purpose is to route different…
Part Number: TMUX6208 Other Parts Discussed in Thread: CD74AC161 , SN74HC161 Hi,
Can you recommend a reference design 4-bit counter that can drive TMUX6208? If none what 4 bit counter is best for TMUX6208?
Thank you.
Regards, May