Part Number: TMUX6213 Tool/software: The datasheet for TMUX6213 has a -3dB specification for +-5V & +-15V supply voltage conditions but only has a response curve for the +-15V condition, which has a lower bandwidth spec. (56MHz vs 135MHz).
I have tried…
Part Number: TMUX6213 Hello Guys,
Good day.
Could you help check if our TMUX6213PWR can be use as a drop-in replacement for Analog Device's ADG1413YRUZ ?
Can they use it without any design changes?
Best regards, Art Mecina Texas Instruments Customer…
Part Number: TMUX7213 Other Parts Discussed in Thread: TMUX6213 Hello,
We are using two TMUX7213s to switch signals driving and sampling two ultrasonic transducers. We drive one at a time and sample the other and then swap.
Some of the transducers…
The following table helps select th e right multiplexer and switch with Mid Voltage 25V =< VSIGNAL =< 99V in different configurations:
Precision , Protection , Automotive , Extended Temperature
Configuration
16:1…