Part Number: TMUX6219 Other Parts Discussed in Thread: XTR200 , TLV61046A Hi,
I am designing a circuit, which multiplexes analog signals and IO Link signals on to the same connector. For one of the connections I chose to switch between the C/Q line…
Part Number: TMUX6219 Hi,
I am currently using the TMUX6219 as an analog switch for voltage pulsing applications, with a maximum voltage of ~17 V. In my setup, EN is held high and I toggle the SEL pin to switch between S1 and S2.
With my current implementation…
Part Number: TMUX6219 Tool/software: I have two questions regarding the MUX chip.
First, which MUX chip should I select? My analog input signals are either ±10V at 0-30kHz or 0-20mA at 0-30kHz. Therefore, I need a MUX to switch between these input signals…
Part Number: TMUX6219-Q1 Other Parts Discussed in Thread: TPS61046 Tool/software: Hi Experts
I am evaluating TMUX6219-Q1 and I have a few queries regarding the power of this IC.
The VDD will be connected to the output of the boost converter TPS61046…
Part Number: TMUX6219-Q1 Tool/software: Hi TI Experts,
I was looking at timing diagrams for this IC and i saw that there is a tr and tf even when they did not talk about it in the specification. May I ask for the actual rise and for time for the 15V…
Part Number: TMUX6219-Q1 Tool/software: Team,
what's the recommended EVM to evaluate this device?
I cannot find an EVM in the Q1 product folder and also not in the industrial product folder.
Best regards
Part Number: TMUX6219-Q1 Tool/software: Hi,
my customer wants to us this device with 12V VDD supply. They would like to feed a 15V signal into S1.
From my understanding, this does not work due to the following specification. Can you confirm?
Thanks…
Part Number: TMUX6219 I have a design that uses the TMUX6219 to provide a PWM gate signal to a floating gate driver as shown below:
The PWM signal is a 3.3V 200kHz signal from an MCU pin with a duty cycle that varies with the VNEG from about 12% to…
Part Number: TMUX6219 Could I use TMUX6219 in scenario such as VDD=5V and VSS=-24V? I don't find clear answer in datasheet.
In this case, does there any other considerations to notice?
If TMUX6219 could not fit the design, could other device make…