Part Number: TMUX6219 Tool/software: I have two questions regarding the MUX chip.
First, which MUX chip should I select? My analog input signals are either ±10V at 0-30kHz or 0-20mA at 0-30kHz. Therefore, I need a MUX to switch between these input signals…
Part Number: TMUX6219-Q1
As the picture shows, the red wine is the leakage line.
Is there such a problem, or what should be paid attention to when designing
Part Number: TMUX6219-Q1 Other Parts Discussed in Thread: TMUX6219 , TMUX7234 , TMUX4052 , TMUX7436F Hi,
In my project, I need to multiplex high voltage interfaces with 100 base ethernet and I was planning to use TMUX6219 for that purpose. S1 inputs of the…
Part Number: TMUX6219 Could I use TMUX6219 in scenario such as VDD=5V and VSS=-24V? I don't find clear answer in datasheet.
In this case, does there any other considerations to notice?
If TMUX6219 could not fit the design, could other device make…
Part Number: TMUX6219 Other Parts Discussed in Thread: TMUX72XXDGKEVM Hi
We have design based on TMUX6219
We need to switch 2 CH 60mA to Output
We try to drive SEL pin with 1.8V (FPGA Pin voltage constraint) with no success
When we drive it with 3.3V…
Part Number: TMUX6219 Customer is looking for a workaround solution on MD system.
In system, they'd like to mux output power between -15V and 0V with 300mA,peak current. We'd like to know if TMUX6219 is workable or not?
application: Gate driver…
Part Number: TMUX6219 Customer tried to transfer the simulation model from Pspice to .TSM(Tina), but it looks it doesn't work. could you offer the .TSM file for simulation. very thanks.
Part Number: TMUX6219 Other Parts Discussed in Thread: TMUX6211 Hello guys,
One of my customers is looking for a analog switch which can be used for RS485 termination resistor connecting and dis-connecting like LTC2873 or MAX13450E. LTC2873 https://www.analog…