Part Number: TMUX6236 Tool/software: Dear TI Team,
We would like to confirm the behavior of the EN pin on the TMUX6236. Is the default state of the ENABLE pin high, meaning the device is enabled by default?
To disable it, we will pull the pin low.
Is…
Part Number: TMUX6236 Tool/software: Hi TI team,
We are currently designing a circuit using the TMUX6236 , and would appreciate your help reviewing our schematic to ensure there are no obvious mistakes or issues.
Thanks!
Part Number: TMUX6236 Hi,
May I know if TMUX6236 can work at 24V? and what about the performance such as continuous current and Rsdon when working at 24V? thanks.
btw, it sounds this part has higher price than Panasonic's solid state relay, it is not…
Hello Harry,
In this situation the device might get damaged. The TMUX6236 is not capable to operate beyond the supply. If the power rail voltage drops below the input voltage, the device will not be able to tolerate it and might won't work.
What is…
Part Number: TMUX6236 Other Parts Discussed in Thread: TMUX7236 This post is made to warn designers wanting to use the TMUX6236 as there is an error in the datasheet. The datasheet was downloaded though the TI website via this link: https://www.ti.com…
Hi Clemens,
Thank you for your support.
Does this happen if the ground levels are different? When testing with the power supply, the ground level was the same. I think it's a problem because it's currently in the board(TMUX6236)-to-board(MCU) test.…
Part Number: TLV9152 Other Parts Discussed in Thread: TMUX6236 Tool/software: Dear TI support team,
Please help me review the schematic of the TMUX6236.
Thanks!
RS-485 voltages cannot go beyond the driver's supplies, but there could be a ground shift between nodes. Can this happen in your application?
RS-232 bus voltages are ±6 V, or more for some other drivers. If you know that the driver at the other end…
Hi Hiren,
The TMUX7236 or TMUX6236 should be the right devices for this use case as they can support 30V supplies and 30V input signals.
Please let me know if there is any other need here.
Regards,
Kameron