Part Number: TMUX7219 I've been observing odd initial behavior from the TMUX7219. By default SA output should be the initial output with IN = 0 as indicated by the datasheet. However, I've noticed with some of the circuits, the initial default is SB despite…
Part Number: TMUX7219 Other Parts Discussed in Thread: LM5171-Q1 , Tool/software: Hi,
I am designing a boost converter. Input source voltage range is 8-16V. Output of boost is 12V with 360A load current. When input source voltage is more than 12V, I…
Part Number: TMUX7219-Q1 Tool/software: Hi Team,
Customer want to use TMUX7219-Q1 to switch -21V and -16V. The design as below:
Please help review the schematic.
Thank you!
Marc
Part Number: TMUX7219-Q1 Other Parts Discussed in Thread: TMUX7308F Dear TI experts,
My customer considers TMUX7219-Q1 for their nest product.
I saw the document below in TI.com ;
https://www.ti.com/lit/ml/slyp783/slyp783.pdf
Is it okay to cover…
Part Number: TMUX7219 Appears to be broken. There were some syntactic differences between favours of SPICE which I edited, but the model didn't work. Some of the code appears to be nonsense when I look at it.
Part Number: TMUX7219-Q1 Other Parts Discussed in Thread: TMUX7219 , LM74700-Q1 , TPS2120 , Tool/software: Hi Team,
In our case, one using scenario is that Vout1 turn on, but Vout2 and VCOM_OPT_R turn off.
Not sure if there is any issue when TMUX7219…
Part Number: TMUX7219 Hi
I will be using this switch in the following configurations
What should be VSS and VDD? Where can I find documentation reflecting the selection of these voltages with regards to the input/output signals?
thanks vadim
Part Number: TMUX7219 Hi,
Regarding the Idd of TMUX7219, Is Idd stable (62uA max , -40 to 125 degree C) regardless of how much current flow through source to drain( or drain to source)of the internal switch?
Or will it vary depend on how much current…