The following table helps select th e right multiplexer and switch with Mid Voltage 25V =< VSIGNAL =< 99V in different configurations:
Precision , Protection , Automotive , Extended Temperature
Configuration
16:1…
What are Overvoltage & Fault events?
An overvoltage or fault event is when a signal with a voltage greater than the maximum rating of the analog switch or multiplexer is fed into the device. These events can occur for many reasons such as EMI from a…