Part Number: TPA0211 Dear Specialists,
My customer is considering TPA0211 and has a question.
I would be grateful if you could advise.
---
According to the datasheet P.17 9.4.1 Shutdown Mode, while in shutdown mode, the device output stage is…
Part Number: TPA0211 Hello,
If the audio output(Vo+,Vo-) with DC removed of TPA0211 shorted to GND,does any protection function work or will it break down?
Best regards,
Manabu Ito
Other Parts Discussed in Thread: TPA0211 , TPA0211EVM TPA0211 datasheet written in "Stereo Single End (SE)".
※Page19
But I think that TPA0211 is Mono SE speaker AMP because of TPA0211 is single input.
Which is correct (Mono or Stereo)?
Or, is…
Other Parts Discussed in Thread: TPA0211 I have recently been using the TPA0211 class AB amplifier to try and power a small speaker. But, After setting it up as in the circuit diagram in the data sheet and as described by the circuit diagram in the user…
Hi, Ben,
We don't have an app note about the pop removal yet. We are planning to release one document about this but it will take some time.
The pop issue can be different from device to device and usually it is related to the impedance mismatch at…
Hi, Saurabh,
Please take a look at these devices below. They support similar features as TPA0103. Please let me know if you have additional questions or comments.
http://www.ti.com/lit/ds/symlink/tpa0211.pdf
http://www.ti.com/lit/ds/symlink/tpa6011a4…
Part Number: TPA6111A2 Other Parts Discussed in Thread: TPA6110A2 , LM4880 , LM4881 , TPA0211
Hello E2E,
I'd like to know the temperature dependence for harmonic distortion for following products.
- TPA6111A2 - TPA6110A2 - LM4880 - LM4881 - TPA0211…
Hi,
Is TPA0211 better for your application? This is a mono amplifier with SE input for both BTL and SE output.
Is there a chance that your application could use two amplifiers, one for the internal speaker and one for the external speaker?
Best…