Hi Ann
Ann Sara Baby said: the IC starts heating up even though no load is connected.
What is the temperature you find with this condition? Even without load, the PWM output will charge/discharge output LC filter, some of the temperature rising is…
Part Number: TPA2005D1-Q1 Tool/software: Hello Expert,
Could this device drive piezo speaker?
I worry that this device is filterless Class-D. so this device's modulation method may be on the premise of connecting the inductive load.
Best regard…
Part Number: TPA2005D1-Q1 Hi,
I have request from Automotive customer to estimate suitable amplifier to drive 50ohm speaker.
Amplifier should be automotive , and 5V power supply
Speakers specifications are follows.
DC resistance:50 ohm
Power…
Part Number: TPA2005D1-Q1 Tool/software: Dear.
We are working on the Risk Assignment document for BOM parts. Therefore, we need information about your products, so please check the attached Excel file and write the information in the red square box…
Part Number: TPA2005D1-Q1 Hi Expert,
Our customer is developing audio with TPA2005D1-Q1. At the begining of playing, a clear click noise can be heard. As below pic shows. Do you have any suggestions about that? Also, any related learning material is…
Part Number: TPA2005D1-Q1 Team,
well, it's all in the title. Should a filter be planned when the speaker is 10cm away and off board (hanging off wires)?
Olivier
Part Number: TPA2005D1-Q1 Other Parts Discussed in Thread: TPA2005D1 , TPA2011D1 , TAS2563 , TAS2562 Hi Expert,
Our customer currently uses TPA2005-Q1 but the output power is not enough. They are looking for replacement. The output power needs to be…
Part Number: TPA2005D1-Q1 Other Parts Discussed in Thread: TLV320AIC3106-Q1 , TPA2005D1 Hi,
I'm planning to use TLV320AIC3106-Q1 audio codec with TPA2005D1-Q1. In data sheet it is given in an image as below in which IN- is positive input.
And…
Part Number: TPA2005D1-Q1 Hello,
my customer wants to use TPA2005D1-Q1 with the single-ended input configuration in order to replace a discrete H-Bridge stage.
The input signal is a PWM (88 KHz) from µC output. Is the IC expected to work with this…